SPC5 studio CAN IDs in the lower section of the ID table don't fire the interrupt.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-19 1:09 AM
I'm using a SPC570S microcontroller and I have 14 CAN IDs in my ID table. Only up to 7 IDs fire the CAN interrupt, however, if I move a lower ID to above 7 it works fine. I have set the number of RX mailboxes to 16 and TX mailboxes to 7
Labels:
- Labels:
-
SPC5 Automotive MCUs
0 REPLIES 0