cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 and using SPC572L we have problem with DPLL channel 16 - SPC5_GTM_DPLL_ACTION_ID_15 not working

Larsa
Associate III

Our SPC572L application are using both MCS1 & MCS2 connected to DPLL and ATOM it works well on all 16 channels except the last one: channel 16 "SPC5_GTM_DPLL_ACTION_ID_15" if we change to ch17 "SPC5_GTM_DPLL_ACTION_ID_16" it runns fine but we need to use all 24 channels soon with the SPC572K device.

0693W00000Dmh8QQAR.jpg0693W00000Dmh8aQAB.jpg 

Is there a known workaround?

/Lars

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ECAST.1
Associate II

Hello,

Errata sheet are available on web-site:

https://www.st.com/en/automotive-microcontrollers/spc572l64f2.html#documentation

Some work around in the DPLL area, one of them could be useful for your issue.

Regards,

Emanuele