cancel
Showing results for 
Search instead for 
Did you mean: 

[Solved] Where to find the test application for SPC560P -DISP?

gl2
Associate III
Posted on March 08, 2015 at 18:11

Hi,

I'm a trainee to STm. I use the SPC560P - DISP board. I've read that in the MCU flash memory there is the test application. I do not know how to run it.

Can anyone help me? Thanks.

#spc5 #studio #spc560p #headers
This discussion is locked. Please start a new topic to ask your question.
17 REPLIES 17
Erwan YVIN
ST Employee
Posted on March 09, 2015 at 09:56

Hello Gianluca ,

on PICTUS Discovery Board ,We have 6 applications on SPC5Studio Wizard (Cf Attachment)

1) you need SPC5xxx SPC5-UDESTK-EVAL Starterkit (4.2 is better) in order to flash an application

Download from

http://www.pls-mc.com/login-a-html?User=SPC5UDESTKUser

2) Plug your your discovery board and install the drivers (FTDI USB)

the drivers

c:\Program Files (x86)\pls\UDE 4.2\Driver\

3) After the compilation ''OK'', you can launch the debug from SPC5Studio and flash the software generated

Best regards

Erwan

________________

Attachments :

2015-03-09_094707.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Kn&d=%2Fa%2F0X0000000bYy%2FLWhxclG6re9.vRXpeLSx5jBnbhMmr2UMK4SCO4_dr24&asPdf=false
gl2
Associate III
Posted on March 09, 2015 at 13:51

Hello Erwan, 

I have the UDE platform and the drivers, but in the ''getting started'' file for this board (SPC560P - DISP) there's written ''Import the test application developed for this board (“Test Application SPC 560P-DISP Discovery Board.zip�)''. Where is this zip? Inside there is a main.c. Without this file does not know how to start.

Then, there is a detailed guide on how to program this board? 

Best regards 

Gianluca

Erwan YVIN
ST Employee
Posted on March 09, 2015 at 17:51

Hello Gianluca ,

From SPC5Studio , Please use the applications coming from Application Wizard

Click on Magic Stick (Cf Screenshot in attachment)

the applications are uptodate

Could you give a screenshot of the ''Getting Started'' of the PLS UDE ?

Best regards

Erwan

________________

Attachments :

2015-03-09_174947.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Qk&d=%2Fa%2F0X0000000bYx%2FKEc3gJAkB.xWhSVsxHAOmNbS5gsFI1fK0ycqFsMhDP8&asPdf=false
gl2
Associate III
Posted on March 09, 2015 at 19:39

I have the getting started for SPC5 studio.

Attached the screenshot.

Ok. This is my board

http://www.st.com/st-web-ui/static/active/en/fragment/product_related/rpn_information/board_photo/SPC560P-DISP%20640x4png

I choose the SPC560P50L5 then Serial and then ChibiOS-RT. But the project contains some errors. For example missing the libraries:

''components.h''

''ch.h''

''shell.h''

''chprintf.h''

Solutions?

Thanks.

Best regards

Gianluca

________________

Attachments :

Immagine.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Qa&d=%2Fa%2F0X0000000bYw%2FnhUC4ejpL_MMmaO0dvS_1aYY.AhebGg9JJ1IvxJCYLQ&asPdf=false
Erwan YVIN
ST Employee
Posted on March 10, 2015 at 11:08

Hello Gianluca ,

After importing the project from the application wizard ,

you need to click on :

1) generate first

2) then compile

have you updated SPCStudio 3.0.0 ==> 3.4.2 from update site ?

                   Best regards

                                     Erwan

gl2
Associate III
Posted on March 10, 2015 at 17:10

Ok it works. Thank you. I have the 3.0 version. I don't know how download the new version.

The last thing, when I put the firmware inside the board, I turn off the board, I plug again the USBand set S1 to ON position. The LedsD11, D12 and D13 should's blinking, but do not work.

Attached the main.c

This is the test file. When I turn on the board the led D1 is red andno leds blinks.

Best regards

Gianluca

________________

Attachments :

main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0QV&d=%2Fa%2F0X0000000bYu%2FTtjA70DT_1Ub6UXZwOuwKcNoNC6SNUnU.m2jVeWElhc&asPdf=false
Erwan YVIN
ST Employee
Posted on March 10, 2015 at 17:35

Hello Gianluca ,

To update SPC5Studio , you need to pass by update site

Help ==> Install new Software (Cf Attachment)

Do not forget to put some proxy settings in Preferences ==> Network

After updating , you should have in Installation Details : (cf Attachment)

On the application ''ChibiOS-RT SPC560Pxx Test Application

for Discovery'' ,

i have no issue ..

Do you use the Debug button (SPC5Studio) to download the firmware by PLS (memtool) ?

Best regards

Erwan

________________

Attachments :

2015-03-10_172319.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I083&d=%2Fa%2F0X0000000bYv%2FRyFxBO4x9A1mxsFAoQCavbMCd7_aMvSP1Oplqy.gjVc&asPdf=false

2015-03-10_172850.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I017&d=%2Fa%2F0X0000000bYt%2FV6hlYegAw0ZGUUvwAiN6nxLebMnPSLwYp7qrMWhZleA&asPdf=false
gl2
Associate III
Posted on March 10, 2015 at 17:53

For the update I have this errors:

will be ignored because it is already installed.

But my version is 3.0.

Yes I make double click in debug.wsx after the build project. When, the UDE visual platform opens and I load the out.elf file. I click on ''program all'' and I wait. The process is successful. I turn off the board and then turn on and It doesn't work.

Erwan YVIN
ST Employee
Posted on March 10, 2015 at 18:40

Hello Gianluca ,

Could you send your full application by exporting it ?

Do you succeed to put a breakpoint in main() function by PLS ?

Serial Port is working ?

   Best regards

                 Erwan