cancel
Showing results for 
Search instead for 
Did you mean: 

Setting up program from scratch ?

AndreasPA
Associate III

Hey All

Fairy new to SPC5 development, coming from st's 32bit standard Micro controllers.

I have a few questions on the process to creating a project from scratch

1) Are we meant to just load the example projects and modify them according to our needs and add anything else OR can we start from scratch via New-> New spc project etcetc...

2)Starting a project from scratch, and adding in the SPC5Studio Pin map editor, i do what i would normal do in CubeMX, save, generate. but from that i just have the platform_component_rla file, and nothing more.

Referring to the help manual, under SPC5STUDIO -> Concepts -> spc5studio Projects

i'm missing my main components /dependencies. Is there a process to installing these into the project that i've missed ?

0693W000000UA3tQAG.jpg

Here is a photo of my workspace.

0693W000000UA3ZQAW.jpg

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

1) if you want to create a project from scratch

New-> New spc5 Project

a) Platform Component matching with your processor is necessary

2) After clicking the platform component, you can add some others compatible components

(Init Package is Meta Package which contains the minimum thing to boot.)

(cf screen shot)

0693W000000UzrBQAS.png

It is possible to reimport Pinmap settings from others projects into your new one and vice-et-versa

Best regards

Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

Hello ,

1) if you want to create a project from scratch

New-> New spc5 Project

a) Platform Component matching with your processor is necessary

2) After clicking the platform component, you can add some others compatible components

(Init Package is Meta Package which contains the minimum thing to boot.)

(cf screen shot)

0693W000000UzrBQAS.png

It is possible to reimport Pinmap settings from others projects into your new one and vice-et-versa

Best regards

Erwan

Ah thankyou !!!

i couldnt figure out how to add those in