2014-11-27 6:02 AM
Hello,
It is a while that I am working on the SPC5Studio with the SPC560B-DIS discovery board.I always had problems connecting to the board using the USB connection.Each time that I couldn't connect, I uninstalled the UDE and re installed it. Not very convenient but it worked.Now nothing works. Can you advice?error report:Message from component 'PpcJtagTargIntf' :Can't connect target !Message from component 'PpcJtagTargIntf' :No JTAG client found !Please check:- target power supply- JTAG cable connection- target configurationMessage from component 'UDEDebugServer' :Unable to establish connection . To correct the situation, check configuration file entries and try again.I am using windows 8.1SPC5Studio ver 3.0.0UDE version 4.02.07Thank you,ShacharSolved! Go to Solution.
2023-08-25 1:38 AM - edited 2023-08-25 1:46 AM
Hello,
to enable VCP you should enable it on device manager cf screenshot
if PLS USB Jtag is not present, maybe your board is ko or in reset escalation.
Do not hesitate to update your PLS Debugger
Download SPC5-UDESTK (pls-mc.com)
Best Regards
Erwan
2014-11-27 6:23 AM
Hello Shachar ,
Your driver PLS USB/JTAG (FTDI) is not installed.The driver is present in the following directory c:\Program Files (x86)\pls\UDE 4.2\Driver\Do not forget to enable VCP (Virtual Com Port) Best Regards Erwan2015-01-05 5:34 AM
Hello Rosen ,
Cf Screenshots Attached In device manager, 1) Check if PLS USB JTAG Adapter for SPC5XXX A / B is well present If not , reinstall from thec:\Program Files (x86)\pls\UDE 4.2\Driver\ 2) From Drivers Properties , Load VCP (Virtual Com Port) 3) Unplug USB cable and replug USB Cable 4) In Device Manager, You should see PLS USB Serial Port (COMX/COMY) I have checked on Windows 8. it is working well. Best regards Erwan ________________ Attachments : Screenshot_-_05_01_2015___11_30_07.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qV5A&d=%2Fa%2F0X0000000bnr%2Fqly7m75_xxwKIr0FffNo7Ospz0Li.15_IpA.OvXDoLM&asPdf=falseScreenshot_-_05_01_2015___11_30_30.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qUOV&d=%2Fa%2F0X0000000bnj%2FMOWSYyXLlpPeaB6r0htS6e6ns4oKV2nkU4ZiQpUms8s&asPdf=falseScreenshot_-_05_01_2015___11_30_53.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qUrD&d=%2Fa%2F0X0000000bnp%2FdJKpaF_dMbD8eDnt6L7XUdS7orz43TKA4Wpuj91YYaw&asPdf=false2015-12-29 3:14 AM
Hello Erwan,
It has been a while, now i bought 2 more boards and unfortunately I am facing the same difficulties as i had with my previous board.Just to remind you,The board is working fine but i can not access it with the UDE.the set up is on an SPC560B-DIS board with SPC560B54L5 controller.12V adapter is connected to the power supply jack.A miniUSB cable connected to the boards and to my LapTop.My LapTop is working with Windows 8.1I am using SPC5Studio version 3.0.0For debugging I am using the PLS UDE version 4.02.07 with the free license for up to 125K.The problem I am facing is that at first (first 2 days) I managed to build and run my application on the board.Then I started to get problems connecting to the board.Then I came to a point that I can no longer connect to the board but my application is still running.My questions are1. Why is it starting OK for a while (1-3 days) and then stop connecting?2. Is there anything to do? 3. What do you mean by enabling VCP?regards,Shachar2023-07-20 12:18 AM
Is the issue resolved or not? We are facing the same problem, so kindly help us with your solution @srosen @Erwan YVIN
2023-08-25 1:38 AM - edited 2023-08-25 1:46 AM
Hello,
to enable VCP you should enable it on device manager cf screenshot
if PLS USB Jtag is not present, maybe your board is ko or in reset escalation.
Do not hesitate to update your PLS Debugger
Download SPC5-UDESTK (pls-mc.com)
Best Regards
Erwan
2023-12-11 2:19 AM
Hello,
I am using SPC574S4 & UDE debugging tool on SPC studio 6.0.
I am getting below error message on windows 11 machine
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
Failed to open communication channel !
Message from component 'FtdiCommDev' :
Failed to open FTDI device driver !
Message from component 'UDEDebugServer' :
Unable to establish connection . To correct the situation, check configuration file entries and try again.
When I connect EVAL board through mini usb port, device manger shows USB serial port & not PLS USB/JTAG adapter
Please suggest solution.
Also
2024-05-17 7:30 PM
i have meet the same problem. enable VCP you should enable it on device manager the way also cannot work!!!
why Failed to open FTDI device driver ! my driver is ok!!!
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
Failed to open communication channel !
Message from component 'FtdiCommDev' :
Failed to open FTDI device driver !
Message from component 'UDEDebugServer' :
Unable to establish connection . To correct the situation, check configuration file entries and try again.
2024-08-26 7:11 AM - edited 2024-08-26 7:12 AM
I am using Windows 11 with UDESTK 5.02.04 Build 8310 version for my SPC560P50. I even enabled Load VCP and tried, but still the board is not connecting. I did verify all the pins on the board and the JTAG connector.
I did reinstall the drivers as well.
Error:
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
No JTAG client found !
Please check:
- target power supply
- JTAG cable connection
- target configuration