2014-09-30 05:45 AM
Hello,
I installed SPC5Studio 3.0.0, and UDE 4.02.05. When i build a new project clicking on ''build all'' icon, SPC5Studio doesn't generate out.elf file, so i am not able to debug. I can debug Software examples for SPC56L-Discovery (dowloaded from the site), because they iclude the correct out.elf file, but if i modify a main.c file, then save and build the project, out.elf isn't updated. Thanks for any useful response. Best Regards Paolo Menoni2014-10-01 12:53 AM
2014-10-01 12:54 AM
Here is the screenshot ;-)
BR Erwan ________________ Attachments : 2014-10-01_094357.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWnD&d=%2Fa%2F0X0000000boX%2FJN014Q1ldSI83iWWWG1WflLBiLQX_lI.Ek849.7cdMk&asPdf=false2014-10-01 02:02 AM
http://www.st.com/web/en/catalog/tools/PF259369#
user.mak is not correctyou have to replace main.c in U_C_SRC# List of all user C source filesU_C_SRC = ./main.c
Sorry for the issue.we will correct the application inside. Best regards Erwan
2014-10-01 06:13 AM
Hello Erwan,
many thanks for the prompt reply.
I followed your instruction (i checked user.mak file, and a imported from the application wizard), but build command doesn't work yet. SPC5Studio doesn't update Out.elf. I have another prolem: when i load the project, ude shows an error, that i attacched to this message. Best regards Paolo Menoni ________________ Attachments : error.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qZ5n&d=%2Fa%2F0X0000000bp6%2F.IBxgOJg6XVm3HDB3ateauJW68Oe_BsNoZoMV1FqfFw&asPdf=false2014-10-01 07:20 AM
2014-10-01 10:09 PM
2014-10-02 01:31 AM
Hello Paolo ,
The generation is OK.The build is KO because of make.exe (PATH Issue).you have a CYGWIN installation in your environment.Your PATH should have this following content :C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\ppc-ht-eabi\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.gnu_1.0.0.201306281422\gnutools;could you give your full installation details ?Help ==> About SPC5StudioButton Installation Details
and Tab Configuration
have you updated into SPC5Studio 3.1.9 ? Normally , this issue is corrected on SPC5Studio 3.1.9Help ==> Install New Software Best Regards Erwan
2014-10-02 11:43 PM
Hello Erwan,
as you requested, i attached a file (configuration.txt) in wich i copied my current spc5 studio configuration. I attached also a file (installnewsw.pdf): in wich i show my proxy setting, and the step i followed to install new software.the third image, i can As you can see in the third image i tested internet connection by using Show View ==> Other ==> Internal Web browser. Unfortunately after i had installed, and had restarted, my version was still 3.0.0, consequently build command didn't work. According to you should I uninstall, and reinstall? Best regards Paolo Menoni ________________ Attachments : configuration.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qYFw&d=%2Fa%2F0X0000000box%2F3qlt3a9dpqaJ8faqDVhho0Cz_.7VtLDubWjeapRdfsY&asPdf=falseinstallnewsw.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qYjc&d=%2Fa%2F0X0000000bp4%2FUFnZxEO2NA0wG8dTgkXTu2Eyp_xWEDuVkgn3c45129E&asPdf=false2014-10-03 12:36 AM
Hello Paolo ,
Your configuration is good. you have already the last version of SPC5Studio. Sorry for the issue. your version is already up-to-date. i am sending to you a document Could you follow the chapter 2 .. Solution in chapter 2.5 and 2.6. if the problem is still present i will send an invitation with teamviewer. Best Regards Erwan ________________ Attachments : SPC5Studio_FAQ_configurations_issue_cx389511_1.0_D2.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qYPN&d=%2Fa%2F0X0000000boz%2FcisdUuIjUBo59hEPiowmLowMAlNm58tSYxxUGtPSWZk&asPdf=false