2014-10-21 5:05 AM
Hello,
I am not able to start SPC5 Studio after it crashes during I worked with the pin map wizard. When I start the application, it only shows me that an error log in the .log has been created. The entry shows me following errors:!ENTRY org.eclipse.core.resources 2 10035 2014-10-21 12:25:17.456
!MESSAGE The workspace exited with unsaved changes in the previous session; refreshing workspace to recover changes.!ENTRY org.eclipse.osgi 4 0 2014-10-21 12:25:17.861
!MESSAGE An error occurred while automatically activating bundle com.st.tools.spc5 (611). !STACK 0How can I repair my workspace or create a new one without re-installing SPC5 Studio?
Best regards,
Patrik2014-10-21 6:25 AM
Hello Patrick,
First of all, backup your application folder in a safe place. (Your application is currently in C:\SPC5Studio\workspace\<your application name>) Then can you provide the following things (as attachments in the reply of this thread )? : - the configuration.xml (in C:\SPC5Studio\workspace\<your application name> folder) - the log file (in C:\SPC5Studio\workspace\.metadata folder) - the name of the application you chose when you started up (for example: SPC560Dxx OS-Less Test Application for Discovery) Best Regards. Ghislain Ballester.2014-10-21 7:47 AM
Hello,
I have several SPC5 projects within my workspace folder. I attached the configuration of the project I worked on when SPC5 Studio crashed. Actually, i was able to open the SPC5 Studio again. I found this solution for eclipse on the internet:<workspace>/.metadata/.plugins/org.eclipse.core.resources/.snap As suggested in a comment: If using Eclipse 4, you may have to delete the file
.metadata/.plugins/org.eclipse.e4.workbench/workbench.xmi aswell. 2014-10-21 8:25 AM
Hello Patrick,
The decorators that you see should be removed if you modify the code analysis policies. This is done as such (see attachment as well) : Open the preferences window: Window/Preferences. Open the Code Analysis section: ''C/C++''/Code Analysis. Make sure that only: potential Programming Problems check boxes are ticked. Regards. Ghislain Ballester. ________________ Attachments : Capture.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWsh&d=%2Fa%2F0X0000000boa%2FUDw89eItwZaQfFovTkzLGUfmMPDcsOipd9HjFVSGlbE&asPdf=false2014-10-21 8:48 AM
Hello!
Thanks, this modification helped. But what was the reason that I didn´t saw the decorators before the SPC Studio crashes? And why shows a new installation of SPC5 Studio on the PC of my colleague the same behaviour? Is this setting part of the project or a general SPC5 Studio setting? Best regards, Patrik2014-10-22 1:46 AM
Hello Patrick,
This setup is related to the workspace you are using. SPC5Studio is installed by default with a predefined workspace (under C:\SPC5Studio\workspace), which is already configured for not showing these warnings. Your colleague may have selected an alternate workspace when starting SPC5Studio. Regards. Ghislain.2014-10-22 7:58 AM
Hello Ghislain,
Ok and is there any way to restore the configuration of the default workspace? Thanks and best regards, PatrikWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.