2017-06-15 11:05 PM
I am working on a CAN bus based project on the SPC560P50L5 platform. The project is based on the CAN RLA example included with the SPC5Studio.
Details about my setup:
My project code size is way less than the UDE debugger EVAL license limit (i.e. 256kB). The size of my project code is as follows:
text data bss dec hex filename
11630 0 2128 13758 35be build/out.elf
When I try to flash the program with UDE debugger I get this error
Fr 16.06.2017 11:17:21.586, Error, MCUManager, License check for trace stream 'Controller0_NexusTrace' error: no valid license for UDE trace add-on found
Fr 16.06.2017 11:17:21.586, Error, MCUManager, Trace stream object 'Controller0_NexusTrace' was removed to due missing license key features
I have tested by using both the external debugger module (SPC5-UDESTK) and the on-board debugger, but in both cases the above error was shown and I couldn't flash the program.
I can confirm that there is no problem with the UDE debugger installation, as I have one another SPC560D40L1 board and UDE is able to flash and debug it just fine.
Is there a way to get around this problem?
Thanks!!
#spc #udeSolved! Go to Solution.
2017-06-16 12:17 AM
Hello Subham ,
you can find the starter kit keys in this following link :
https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html
For your information, it is better to use
UDE debug kit version
4.08.xxBest Regards
Erwan
2017-06-16 12:17 AM
Hello Subham ,
you can find the starter kit keys in this following link :
https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html
For your information, it is better to use
UDE debug kit version
4.08.xxBest Regards
Erwan
2017-08-09 1:20 PM
Hello,
SPC5-UDESTK does not allow to do NEXUS trace. Therefore These warnings are output. If you like to get or use NEXUS trace please contact PLS directly: