cancel
Showing results for 
Search instead for 
Did you mean: 

License check for trace stream failed for SPC560P50L5

Subham Roy_O
Associate
Posted on June 16, 2017 at 08:05

I am working on a CAN bus based project on the SPC560P50L5 platform. The project is based on the CAN RLA example included with the SPC5Studio.

Details about my setup:

  1. SPC5Studio version 5.3
  2. UDE debug kit version 4.02.07 (SPC-UDESTK-EVAL license)
  3. SPC5-UDESTK JTAG debugger (

    http://www.st.com/resource/en/data_brief/spc5-udestk.pdf

     )
  4. GNU FreeGCC compiler with VLE

My project code size is way less than the UDE debugger EVAL license limit (i.e. 256kB). The size of my project code is as follows:

text    data    bss    dec    hex filename

11630      0   2128  13758   35be build/out.elf

When I try to flash the program with UDE debugger I get this error

Fr 16.06.2017 11:17:21.586, Error, MCUManager, License check for trace stream 'Controller0_NexusTrace' error: no valid license for UDE trace add-on found

Fr 16.06.2017 11:17:21.586, Error, MCUManager, Trace stream object 'Controller0_NexusTrace' was removed to due missing license key features

 

I have tested by using both the external debugger module (SPC5-UDESTK) and the on-board debugger, but in both cases the above error was shown and I couldn't flash the program.

I can confirm that there is no problem with the UDE debugger installation, as I have one another SPC560D40L1 board and UDE is able to flash and debug it just fine.

Is there a way to get around this problem?

Thanks!!

#spc #ude
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on June 16, 2017 at 09:17

Hello Subham ,

you can find the starter kit keys in this following link :

https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html

 

For your information, it is better to use 

UDE debug kit version

4.08.xx

    Best Regards

                   Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee
Posted on June 16, 2017 at 09:17

Hello Subham ,

you can find the starter kit keys in this following link :

https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html

 

For your information, it is better to use 

UDE debug kit version

4.08.xx

    Best Regards

                   Erwan

Matthias Noack
Associate II
Posted on August 09, 2017 at 22:20

Hello,

SPC5-UDESTK does not allow to do NEXUS trace. Therefore These warnings are output. If you like to get or use NEXUS trace please contact PLS directly:

http://www.pls-mc.com