2020-01-14 03:12 AM
I newly get a SPC56B-Discovery board. I have installed the SPC5Studio and UDE STK 5.0 on my PC. I select an example project and build OK with SPC5Studio. Then I connect the board to PC with USB cable. The PC can recongnize "PLS USB JTAG Adapter for SPC5XXX A / B" and I enabled the VCP function referred to this link:
https://community.st.com/s/question/0D50X00009XkgOu/problems-with-ude-visual-platform
Then I unplug and plug the USB cable, the VCP COM ports occur, the drivers seems OK now, and the preloaded blinky program works fine on the board. But when I load debug.wsx from the example project with UDE STK 5.0, it gives these errors as same as the link above:
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
No JTAG client found !
Please check:
- target power supply
- JTAG cable connection
- target configuration
All jumpers are in the default config. Do you have any sugession?
Thanks!
2021-09-17 01:03 AM
I have the same problem as mentioned by the user above. UDE STK 5.0 and Windows 10.
All the drivers are installed properly and the Load VCA settings are ticked.
I am getting the same error though.
Has this issue been solved?
Thank you!