cancel
Showing results for 
Search instead for 
Did you mean: 

I wanted to know JTAG PIN details of the SPC5-UDESTK-PLUS Debugger

Sk1
Associate

Hi All,

I am unable to connect target to the UDE.

1)Is there any necessity to install virtual Com port drivers for debugging with UDE-STK-PLUS debugger apart from the drivers provided by the UDE software ?

2) How to integrate SPC5 studio with UDE-STK-PLUS ?

3) Also, please share  JTAG PIN details of the SPC5-UDESTK-PLUS Debugger. So that I can verify the target connection with UDE-STK-PLUS.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee

Hello Sk ,

1) No, Virtual Com Port drivers are only useful to use Serial Port (using printf mecanism)

2) There are "UDE Eclipse 4 integration" in http://spc5tools.spc5studio.com/

you can install it

but PLS UDE should be installed in your PC

3) Which board do you use ? i think that the information is in the datasheet

Best Regards

Erwan