2020-11-21 06:43 AM
Hello,
I am currently trying to run a Machine Learning application on the SPC584B-DIS MCU. I used SPC5Studio with the AI plugin to create the project and it compiled without an error. The board is connected to the PC by USB cable. When I try to validate the project on the board however, I always receive the error: "LOAD ERROR: STM32 - no connected board(s), invalid firmware or the board should be re-started."
From the manual (https://www.st.com/resource/en/user_manual/dm00532742-spc584bdis--discovery-board-stmicroelectronics.pdf) I understand that I need to set the jumpers in a certain way to enable the communication between the board and a host. I am fairly new to embedded programming however, so I don't understand how to set these jumpers properly so I can communicate with the board. Can someone help me understand?
Best regards
Solved! Go to Solution.
2020-11-30 01:52 AM
Hi,
this error occurs when the Validation is enabled. I suppose you have loaded one of the AI example containing in SPC5Studio for the SPC584B-DIS and you have enabled the Validation in the related tab within the SPC5-AI Component. The error can occur when:
Please, could you check that you are not in one of the previous cases?
In the meantime, please, let me also share the SPC5Studio-AI User Guide, in which you can find more details about how to use the SPC5-AI Component.
Regards,
Luigi
2020-11-30 01:52 AM
Hi,
this error occurs when the Validation is enabled. I suppose you have loaded one of the AI example containing in SPC5Studio for the SPC584B-DIS and you have enabled the Validation in the related tab within the SPC5-AI Component. The error can occur when:
Please, could you check that you are not in one of the previous cases?
In the meantime, please, let me also share the SPC5Studio-AI User Guide, in which you can find more details about how to use the SPC5-AI Component.
Regards,
Luigi