2023-01-26 05:05 AM
The FlexRay cluster I have here consist of 2 FlexRay cold-start nodes and the third node, spc58ec mcu non-cold start node. Can anybody suggest what can go wrong ?
2023-02-07 10:57 PM
I also want to use the FlexRay, Is this code write by yourself or transplant from other project?
2023-02-23 08:15 AM
Hello Sebastian ,
Have you solved your issue ?
it could be due to the loss of synchronization with the network.
Best Regards
Erwan
2023-02-23 09:02 PM
Hello,
Yes. It has been resolved. The issue was with the MCR register's configuration. After correctly setting the MCR register, I reached the expected protocol state normal active.
Thanks and kind regards,
RSeba
2023-02-24 01:39 AM
Hello,
Currently I am doing the transmit buffer configurations. I configured 2 transmit buffers. But the FLEXRAY_0.CH[1].MBIDXR.B.MBIDX field is still 0 even after setting an index. Do you know why is it so ?
Kind regards,
RSeba