2024-10-10 11:47 AM
I have flashed the application onto the HSM core of SR6G7, and I can see that the HSM core is not running up without a trigger from the Host core. After some analysis, I found that the HSM core requires a power mode change from DRUN mode to RUN mode via the ME_MCTL register. Therefore, I would like to know how we can enable the HSM core to run first by changing the ME_MCTL register value to RUN mode directly, without running the Host core of SR6G7. I want to ensure HSM core running first before host core running. Any help would be appreciated.