2023-06-26 4:38 AM
I'm using SPC58EC80 (SPC58EC DISP). I have coded the MCU for standby mode. It's working well but I have program it like wheather the MCU is booting from power ON or from standby wakeup. I have four wakeup intterupts and I want to know which wakeup interrupt is triggered the MCU to wakeup.
Solved! Go to Solution.
2023-07-11 10:46 PM
ease have a look at RGM module, FES and DES registers.
These registers are used to understand if the device is booting from a Power On Reser of a Functional/Destructive reset or from a Wakeup condition.
Regards.
2023-07-11 10:46 PM
ease have a look at RGM module, FES and DES registers.
These registers are used to understand if the device is booting from a Power On Reser of a Functional/Destructive reset or from a Wakeup condition.
Regards.