cancel
Showing results for 
Search instead for 
Did you mean: 

How to change mcuconf.h values in the code generator?

aurelien23
Senior
Posted on June 26, 2015 at 15:34

Hello,

I always have to manually change some values in mcuconf.h when I generate the code out of the config because I can't find how to set them in the config or anywhere else.

I'm using a 16MHz external xtal and I have to set SPC5_FMPLL0_IDF_VALUE and SPC5_FMPLL1_IDF_VALUE to 2 instead of the default 5. Same for SPC5_MCONTROL_DIVIDER_VALUE that I have to set to 15 instead of 1 to get my ICU-PWM config to work. Where can I set these value in the config to get correct values on code generation?

Thank you for all improvments since the v2.0
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Erwan YVIN
ST Employee
Posted on June 26, 2015 at 16:27

hello Aurelien ,

mcuconf.h is generated from the configuration file.

HAL Drivers ==> Initialisation settings ==> FMPLL0 Settings 

Best regards

                 Erwan

aurelien23
Senior
Posted on June 29, 2015 at 08:53

Hello,

Oops, I never noticed it was collapsed...

Thank you!