2017-10-26 12:07 AM
How could I read out the hex file from SPC560P34L1CEFA?
#hex2017-10-26 1:10 AM
Hello Zhang ,
Yes , it should be ok for an uncensored chip.
for a censored one , you need the password.
You should take the hand with a debugger
Example : for PLS , there is a Macro SaveHex <file> <range>
I have never tested this feature.
Best Regards
Erwan
2017-10-26 8:41 PM
I got the following information:
'_______________________________________________________
'' SaveHEX command line function' ' generates intel-HEX file '' command line SaveHex output-file range1 [range2] [range3] .....' range description:' <startaddress>,<length> '_______________________________________________________Sub SaveHEX(File,ParameterObj)
set debugger = workspace.Coredebugger(0)
set DisASMObj = debugger.DisASMObj If Not IsObject(ParameterObj) Then MsgBox ''Number of parameters wrong'' Exit Sub End If If IsNumeric(File) Then MsgBox ''File parameter wrong - '' & File Exit Sub End If DisASMObj.OutputPath = CStr(File) bRetVal = DisASMObj.CreateStream(True,''UDE generated intel-Hex file of current Program'',False) If bRetVal = True Then ParmeterCnt = ParameterObj.ParameterCount If ParmeterCnt = 0 Then MsgBox ''Number of parameters wrong '' & ParmeterCnt Exit Sub End If If ( ParmeterCnt Mod 2 ) <> 0 Then MsgBox ''Number of parameters wrong '' & ParmeterCnt Exit Sub End If RangeCnt = ParmeterCnt/2 ParamIndex = 0 For Range = 0 To RangeCnt -1 Address = CLng(ParameterObj.Parameter(ParamIndex)) Length = CLng(ParameterObj.Parameter(ParamIndex +1)) ParamIndex = ParamIndex +2 DisASMObj.AddRange Address,Length,0 Next DisASMObj.HexFileModeFlag = True DisASMObj.WriteAllRanges(False) End IfEnd Sub
In the following, what should I insert into it? Could I insert something into it like this ''Application.hex 0x0~0x7FFF''?
2017-10-26 9:04 PM
The instructions suggest something more like
SaveHEX Application.hex 0,0x8000
2017-10-26 9:13 PM
I do it like this: Application.hex 0x0,0x8000
and I got the following error.
2017-10-27 1:39 AM
Hello Zhang ,
You have to run the script
there is a button to do that
and check the Windows directory
Best regards
Erwan
2017-10-27 2:38 AM
Hello Zhang ,
You should enter Application.hex,0x0,0x8000
the hex file will be in c:\windows directory.
Are you administrator of your PC ?
Best regards
Erwan
2017-10-27 2:59 AM
Yes, I'm the administrator of my PC and I can install some software in my PC. I enter ''Application.hex,0x0,0x8000'' and after the following it will go to the end.
2017-10-27 3:50 AM
I use the following buttons and there is no Application.hex in the Windows directory.
2017-10-27 7:01 AM
Hello Zhang ,
No , You should run the macro script not the embedded software.
Best regards
Erwan