2022-06-30 7:08 PM
Solved! Go to Solution.
2022-07-01 1:24 AM
Hello,
in SPC5Studio, click on select you product family:
select a product and click on next:
select a driver example:
and finally select the demo application and click on finish:
It is the same answer for any driver example, any product family
Best regards
2022-07-01 1:23 AM
hello ,
Which MCU do you use ?
please check the test Application in SPC5 families in SPC5Studio (ADC part)
Best Regards
Erwan
2022-07-01 1:24 AM
Hello,
in SPC5Studio, click on select you product family:
select a product and click on next:
select a driver example:
and finally select the demo application and click on finish:
It is the same answer for any driver example, any product family
Best regards
2022-07-01 1:27 AM
Hi Erwan,
i'm using SPC57 (SPHAERO). Which one i need to select?
2022-07-01 1:30 AM
what is different between "saradc_lld_cfg.h" and "adc_lld_cfg.h"? i got confuse between these two.
2022-07-01 1:53 AM
saradc_lld_cfg.h is the only one used on SPHAERO product, do not mind about other.
2022-07-01 2:03 AM
What means by {8U,9U} and {0U,0U} ? One more thing whats is "anp" stand for and function?.
2022-07-01 2:16 AM
be careful, you are not looking to the SPHAERO demo (SPC574S) but to the VELVETY one (SPC570S) do you confirm you product is SPC574S ?
2022-07-01 2:18 AM
U is used to define unsigned immediate for MISRA purposes
anp, I suppose it stands for analogue port ? as it is used to select analogue channels
2022-07-01 2:23 AM
oh i think i wrongly open the VELVELTY one. is it this one for sphaero line (ref pic i send) ? yes i confirm my product is spc574s