cancel
Showing results for 
Search instead for 
Did you mean: 

Filter and Mask configuration of FlexCAN for SPC560

YLin.2
Associate II

Hi,

I can't find any document that defines the Filter and Mask for FlexCAN, so I post a question about it.

I think the filter only passes frames that contain exact ID as the ID in ID mask field. Am I right?

0693W000005BDKVQA4.jpgBest regards

Yuechuan Lin

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
DCARR
Associate III

Hi,

YES you are right.

The CAN controller is configured to use the RX global mask that is set to 0x0FFFFFFF

Best regards

Domenico

PChia.2237
Senior

Is possible to change or just check this RX global mask?

Because i have a problem in standard RX that seams that filter mask is not 0x7FF , but 0x3FF.

I have tested in this way:

RX ID= 0x1

up to message id 0x201 -> 0b 0010 0000 0001 filter works

if i send message id 0x401 ->0b 0100 0000 0001 filter not works, because i i receive the message.

Best Regards,

Patrick

PChia.2237
Senior

I have solved replacing in can_lld.h

canp->flexcan->RXGMASK.R = 0x0FFFFFFFU;

with

canp->flexcan->RXGMASK.R = 0xFFFFFFFFU;