2020-10-28 11:13 PM
We are selecting a controller for our new Automotive project with CAN - FD connectivity, but we want to know whether ST provides the driver stack for CAN - FD for above microcontrollers for free.
Solved! Go to Solution.
2020-11-02 03:53 AM
Hello,
have a look at SPC5Studio (www.st.com/spc5studio).
It includes CAN-FD driver fro SPC57 and SPC58 devices.
SPC56 devices do nt have CAN-FD
For STM32G4, please ask to STM32 section.
Regards,
Giuseppe
2020-11-02 03:53 AM
Hello,
have a look at SPC5Studio (www.st.com/spc5studio).
It includes CAN-FD driver fro SPC57 and SPC58 devices.
SPC56 devices do nt have CAN-FD
For STM32G4, please ask to STM32 section.
Regards,
Giuseppe
2020-11-02 04:42 AM
On the STM32 the examples are typically low level peripheral code, for real drivers and stacks you'll like need to find or port ones with the features you want.
2020-11-03 05:15 AM
Thank you for your valuable reply. But SPC560D controllers are with FlexCAN.
Are FlexCAN and CAN-FD same?
2020-11-03 05:18 AM
STM32G431CBT3 controllers are supporting CAN-FD interface. For this device, does ST provides the driver stack for CAN-FD?
2020-11-13 08:11 AM
CAN-FD and FlexCAN are not the sane
FlexCAN support CAN protocol but does not support CAN-FD protocol.
If you are looking at automotive microcontrollers with CAN-FD please have a look at SP57/SPC58 family