2020-10-20 8:04 AM
What does it mean CUT?
I suppose is a CPU identification tag, but I'm not sure.
I developing a project with SPC5 studio V.6.0, but I don't understand which file I must include in my project between spc574k_cut24.h and spc574k.h.
I see there are some example for CUT 2.3 and CUT 2.4 but I don't known the differences.
Can anybody help me, please?
Thank you very much.
Best regards
E.
Solved! Go to Solution.
2020-11-02 4:54 AM
Hello,
the register SIUL_MIDR1 contains the information you are looking for.
Regards,
Giuseppe
2020-10-21 2:40 AM
Hello ,
CUT is an hardware version. (2.4 is more recent than 2.3)
A different hardware can impact the include file (registry file).
a simple diff , you can see the difference in term of IPs or registry.
normally , some basic example should work on the 2 cuts.
Best regards
Erwan
2020-10-21 5:03 AM
Hello,
thank yuo very much for the quick reply.
But where can I found in the ST documentation, what CUT can I use with my devices? (now I'm developing on SPC574K72E5).
For example, in SPC5Studio I can find two CAN examples, one for CUT 2.3 an one for CUT 2.4. Which example can I use for the SPC574K72E5?
Best regards
E.
2020-11-02 4:54 AM
Hello,
the register SIUL_MIDR1 contains the information you are looking for.
Regards,
Giuseppe