2024-11-01 03:17 AM
Dear community members,
There are multiple functions related to cell balancing in AEK-POW_BMS63EN_id. However, when I tested, none of them work. Here is my main code based on the "SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_14Cells_GUI application for discovery" example. Could anyone experts give me documents about how to manually use cell balancing of this board? and explain detail how cell balancing of AEK-POW-BMS63EN works?
This is my code:
And this is the results: Cells balancing still turn on
Solved! Go to Solution.
2024-12-02 02:12 AM
Hi Trishuynh,
It seems you entered in a faulty condition; this may be related to some poorly connected wire. I invite you to follow these steps:
I also suggest to take a look to UM3185 for a better understanding on how to use our BMS boards.
The Demo we suggest to use with the new library (BMS_CHAIN) is SPC58EC - AEK_POW_BMS63EN_SOC_Est_SingleAccess_CHAIN
Thanks,
AutoDevKit Team.
2024-12-03 03:12 AM - edited 2024-12-03 03:13 AM
Dear ATROI,
Thank you so much. Back to the balancing of the new driver, I found out that only two value that can change the balancing status of the system (in the void AEK_POW_BMS63CHAIN_app_parserData(void)):
AEK_POW_BMS63CHAIN_app_dataChain[AEK_POW_BMS63CHAIN_chainidx].AEK_POW_BMS63CHAIN_nodeData[AEK_POW_BMS63CHAIN_devidx - 1].AEK_POW_BMS63CHAIN_Pack_Enable_Bal = 1;
AEK_POW_BMS63CHAIN_app_dataChain[AEK_POW_BMS63CHAIN_chainidx].AEK_POW_BMS63CHAIN_nodeData[AEK_POW_BMS63CHAIN_devidx - 1].AEK_POW_BMS63CHAIN_Pack_Enable_Discharge = 0;
When I changed the AEK_POW_BMS63CHAIN_Pack_Enable_Bal to 0, the balancing for each cell turned off to 0.
When I changed the AEK_POW_BMS63CHAIN_Pack_Enable_Discharge to 1, the balancing for each cell turned on to 1.
However, All the below function seems do not works in any situation or I do not know how and when to put it in the code.
//Set Balancing Mode of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_setBalMode
//Enable Balancing Cell of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_enableBalCell
//Disable Balancing Cell of Node of BMS Chain
- AEK_POW_BMS63CHAIN_node_disableBalCell
//Set Balancing Start of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_setStartBal
//Set Balancing Stop of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_setStopBa
Could you please guide me by providing some example code to manually control balancing of each cell (turn on, turn off).
Thank you for your attention to this matter. I appreciate your assistance in clarifying this detail.
Best regards,
Trishuynh.
2024-12-25 01:04 AM
Dear Experts,
As in the document and figure, the on-chip MOSFETs are switched on to sink a current from the cell, thus dissipating charge on RDIS. So I want to ask that if balancing status of cell 1, 2, 3 ,4, 5 is on (value is 1) => the on-chip MOSFET of pin S1 S2 S3 S4 S5 are switched on right? I dont know how to know that the on-chip MOSFETs are switched on or off and how to control them?
Thank you for your attention to this matter. I appreciate your assistance in clarifying this detail.
Best regards,
Trishuynh.