cancel
Showing results for 
Search instead for 
Did you mean: 

STA350BW: 2ch downmix to 1ch (Mono) with OCFG ''00''

florian2
Associate
Posted on January 21, 2014 at 12:32

Hello,

Planed: 1 integrated Speaker, 1 external Speaker.

If external Speaker is not connected, the internal one should play ''Mono''.

The configuration will remain ''2-channel (full-bridge) power, 2-channel data-out'' OCFG ''00''

In AP-Workbench and Datasheet, i did not found any Switch to generate ''Mono'' from 2-channel Input, with STA350BW.

Would this be possible using the PEQ? Post-Mix?

Are there additional Documents?

How can i configure this: (CH1+CH)/2 ?

Thank you best regards,

Florian Breu

#mono-downmix-sta350bw
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nickname1623_O
Associate II
Posted on January 22, 2014 at 03:08

hello Florian,

for this purpose, you need to implement pre mixer by mix coefficients setting .

for example , when channel 1 had been used for integrated speaker , and when external speaker is absent, you need to set mix coefficients of channel 1 to CH1=400000 , CH2=400000, mix coefficients of channel 2 to CH1=000000, CH2=000000. due to 7FFFFF is equal to 1 , so 400000 is equal to 0.5 in STA350BW DSP.

Thanks and best regards

Yun Tao ZHAO

From: breu.florian.001

Posted: Tuesday, January 21, 2014 12:32 PM

Subject: STA350BW: 2ch downmix to 1ch (Mono) with OCFG ''00''

Hello,

Planed: 1 integrated Speaker, 1 external Speaker.

If external Speaker is not connected, the internal one should play ''Mono''.

The configuration will remain ''2-channel (full-bridge) power, 2-channel data-out'' OCFG ''00''

In AP-Workbench and Datasheet, i did not found any Switch to generate ''Mono'' from 2-channel Input, with STA350BW.

Would this be possible using the PEQ? Post-Mix?

Are there additional Documents?

How can i configure this: (CH1+CH)/2 ?

Thank you best regards,

Florian Breu