2014-01-14 6:22 AM
The launch wizard panel of the APWorkbench tool is referring to an APWLink interface, can you please tell more about?
2014-01-15 8:26 AM
The ''APWLink Audio Interface'' panel on the APWorkbench launch wizard allows to use the
http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF253187
as a general purpose I2C interace with scripting capabilities and I/O controls. I2C operations can be instructed through a user-friendly console window, including logging capabilities. Script files are supported as well. The APWLink also offers onboard ADC and SPDIF receiver devices which can be used to feed audio data to digital audio amplifiers such as, for instance, .