cancel
Showing results for 
Search instead for 
Did you mean: 

STA311B - RESET pin behavior

spam9986
Associate
Posted on April 05, 2016 at 18:58

Hello,

Does the RESET pin have an internal pull-up?

It seems that there's always ''0'' on RESET pin when it's floating on my STA311B... And it sinks up to 15 mA when I'm trying to pull it up to VCC with external resistor. Does it mean that my STA311B is toast? Could it be the consequences of phantom power given to RESET pin while the main supply to VDD was down?

#reset #sta311b
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nickname1623_O
Associate II
Posted on April 06, 2016 at 03:10

hi Omalay,

it's a schmitt trigger buffered input . so will not sink such high current normally .

usually a 10K ohm pulled up resistor was enough for reset pin , and you also need to add a 1nF MLCC chip capacitor nearby IC pin to prevent unexpected reset by ESD or noise from ground .

Thanks

YT