cancel
Showing results for 
Search instead for 
Did you mean: 

STA309a stereo input to 2.1 output

js
Associate
Posted on September 24, 2015 at 16:06

Hi!

STA309a documentation is little bit lacking on this topic, so some explanation is needed.

Required configuration:

Single stereo I2S input on SDI12

Two I2S outputs: stereo to main speakers and mono to subwoofer

Questions:

1. What is the correct output I2S mapping: SDO12 to main speakers and SDO56 to subwoofer (right or left)?

2. Can you tell if the following configuration is correct?

AMBMME and AMBMXE bits enabled (bass mix and crossover)

CSS and RSS set to 10 (off)

SUB enabled

FSS and XO bits sets according to speaker configuration

Thanks!

#sta309a
1 REPLY 1
Nickname1623_O
Associate II
Posted on October 22, 2015 at 10:54

Hi JSLV ,

Normally the channel configuration was  channel 1/2 for main channel ( left and right ) , channel 3/4 for rear channel ( rear left and right ) , channel 5/6 for center and woofer .

the setting is right ,but those configuration had been used for 6 channel input according to dolby digital specification , then if only 2 channel input was available , the output must be adjusted .

due to mixing setting was not matching .

Thanks ,

YT