Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Special IC

Posted on November 08, 2015 at 19:24Anyone heard about a ST IC with the name 07502233?It sits in a Bosch Charger with a LM324AN beside it. Both are STMicroelectronics. But I can't find what type the 07502233 IC are! Any that know and can tell if it'...

geir by Associate
  • 2620 Views
  • 1 replies
  • 0 kudos

One of the LMV324IDT op amps as a comparator

Posted on November 03, 2015 at 17:13We have an extra op amp in the quad package that we'd like to use as a comparator to save cost.  Any recommendations?  I'm a little concerned about stability and oscillations.

Evaluation board for TDA7801

Posted on October 19, 2015 at 18:30Hi, I'm looking for a class AB amplifier with integrated DAC and I2S bus and I found STm TDA7801. I'm a teacher and I would like to use this device at school for some projects. Unfortunately, I have no sufficient a...

STA309a stereo input to 2.1 output

Posted on September 24, 2015 at 16:06Hi! STA309a documentation is little bit lacking on this topic, so some explanation is needed. Required configuration: Single stereo I2S input on SDI12 Two I2S outputs: stereo to main speakers and mono to subwoo...

js by Associate
  • 1087 Views
  • 1 replies
  • 0 kudos

Choosing a power supply for an ST510A device

Posted on July 17, 2015 at 23:24Hello,I'm setting up a system with a STA309A DSP and a STA510A amplifier.I'm expecting to connect two 8Ω loads with a maximum power of 50W each, but I can't find the graphics that show the estimated Power dissipation ...

jorge by Associate II
  • 2365 Views
  • 5 replies
  • 0 kudos

STA369BWS output configurations

Posted on September 04, 2015 at 23:14Hi, I'm using STA369BWS as the amplifiers in my application. There are a pair of stereo speakers and a subwoofer speaker. The stereo speakers' resistance is 4 OHM, and the subwoofer one is 8 OHM. I'm using two ST...

winston by Associate
  • 783 Views
  • 0 replies
  • 0 kudos

TDA7576B input voltage

Posted on August 28, 2015 at 15:47Hello,I am developing new device with TDA7576B amplifier. TDA7576 input voltage -0.3 to 5V (from absolute maximum ratings). Is it rms value or input signal voltage must be positive only? I need computer line out sig...

sta339bw 12MHZ

Posted on August 27, 2015 at 09:31A amplifier system:ADC+STA339BW+MCU,MCU generate a 12MHz clock apply to ADC(connect to MCLK pin) and STA339BW(connect to XTI pin)。I don't know how many differences will be,will this effect THD+N,SNR? is there any do...

331912674 by Associate II
  • 1140 Views
  • 1 replies
  • 0 kudos