cancel
Showing results for 
Search instead for 
Did you mean: 

Operating voltage vs absolute maximum ratings

z58
Associate
Posted on June 11, 2012 at 16:34

I plan to use the comparator TS3021 with Vcc = 5V+/-2%. Will it be OK? The data sheet shows the recommended VCC 5V max and absolute max = 5.5V. We will have Vcc = 4.9V min and 5.1V max. Is it acceptable for the reliable TS3021 functionality? 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nickname14663_O
Associate II
Posted on June 14, 2012 at 17:31

Hello Mirmon,

The TS3021

will still operate, but please note that all parameters (Min/Max) are specified at Vcc = 5V. 

Regards,

Sylvain