cancel
Showing results for 
Search instead for 
Did you mean: 

I've installed the APWorkbench suite but I'm getting the following message when launching the application: ''APWorkbench I/O warning: No FTDI driver found, APWLink communication will be disabled…..''. Can you please provide more explanation about?

nmagniez
Associate II
Posted on February 07, 2014 at 10:08

I've installed the APWorkbench suite but I'm getting the following message when launching the application: 'APWorkbench I/O warning: No FTDI driver found, APWLink communication will be disabled…..'. Can you please provide more explanation about?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
5 REPLIES 5
Marco VENERI
Associate II
Posted on February 07, 2014 at 10:21

The

http://www.st.com/web/en/catalog/tools/PF253187

is used to communicate with Sound Terminal evaluation kits and requires a third-party driver to operate correctly. Driver is available from

http://www.ftdichip.com/Drivers/D2XX.htm

.

Though FTDI driver is already included in the APWorkbench setup package its installation will be completed only once an actual APWLink I/F is connected to the PC, via USB. If this does not happen the communication with such I/F will be disabled.

Note that APWorkbench can still be operated either in simulation mode (no communication with any actual IC/device) or through an

http://www.st.com/web/en/catalog/tools/PF258331

, if available. Also, STAudioHub interface is recommended for ST MEMS Microphone evaluation.

miguelernandez
Associate
Posted on April 09, 2014 at 11:48

depends on your windows you maybe have to install the drivers manually, even if windows thinks the drivers are okay then apworkbench will not find them

jthuot
Associate
Posted on July 14, 2014 at 17:37

Hi,

I'm experiencing the same issue with the FTDI drivers.

Any luck on that front?

Thank you,

Jonathan

jthuot
Associate
Posted on July 15, 2014 at 16:16

I have installed the drivers manually under Win7(64) with APworkbench(64), still not found.

Any suggestion on what to do next?

Marco VENERI
Associate II
Posted on July 18, 2014 at 15:42

Jonathan,

Make sure to download and install the proper driver version for your OS (64 bits) from the FTDI site.

Also, the driver installation will be completed only after an actual STAudioHub board will be plugged on the USB port.

Marco