cancel
Showing results for 
Search instead for 
Did you mean: 

How to determine TS391 output voltage

Central SUPPORT
Senior II

In TS391 datasheet for max. Vol output voltage two values are specified:

0690X000006Dw0RQAS.png

Under which conditions is 400mV resp. 700mV valid?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

More information about output voltage can be found in figure 7 of datasheet. You can see that output voltage also depends on the current. Once the output transistor cannot be hold in saturation, the output voltage will start to rise rapidly. As long as the output current is below 1mA transistor will be in saturation and Vol should be under 700mV under all operation conditions.

0690X000006Dw1oQAC.png

View solution in original post

1 REPLY 1
Central SUPPORT
Senior II

More information about output voltage can be found in figure 7 of datasheet. You can see that output voltage also depends on the current. Once the output transistor cannot be hold in saturation, the output voltage will start to rise rapidly. As long as the output current is below 1mA transistor will be in saturation and Vol should be under 700mV under all operation conditions.

0690X000006Dw1oQAC.png