cancel
Showing results for 
Search instead for 
Did you mean: 

HardFault_Handler upon updating variables inside DMA Callback

DCont.1
Associate II

Hi,

I am currently implementing a guitar effects pedal using the STM32F446RE and the PCM3060 as my CODEC.

I have gotten everything to work, except when I try to adjust the following parameters

cf0_lim = (int)(time*l_CB0);

cf1_lim = (int)(time*l_CB1);

cf2_lim = (int)(time*l_CB2);

cf3_lim = (int)(time*l_CB3);

ap0_lim = (int)(time*l_AP0);

ap1_lim = (int)(time*l_AP1);

ap2_lim = (int)(time*l_AP2);

inside my DMA. For some reason, I cannot update this parameters anywhere in my code. I tried updating them outside of the DMA callbacks for my CODEC and also on the while loop.

I am pretty sure these are the parameters that are triggering the HardFault error because whenever I comment them out the code runs fine.

I am able to update the "time" and "wet" variables whilst the DMA is running. This is fine, however, without updating the cfx_lim and apx_lim variables, I can't do much to apply this changes to the current effects that are being used for the reverb effect.

Is there a reason why this is happening? I have attached my entire code.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
0 REPLIES 0