cancel
Showing results for 
Search instead for 
Did you mean: 

Difference between LM224 and LM224A

gene-zhen
Associate
Posted on November 28, 2014 at 09:04

Hi,

Is there tmeperature drift difference between the two types? Or is there any other difference between the two type,please?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nickname560_O
Associate II
Posted on November 28, 2014 at 11:38

Hi wang.zhen.003,

For most of ST operational amplifier product the A label define a product with a better Vio.

You don’t have any difference one the DVio/DT = 7µV/°C in typical value or 30µV/°C for max value in the both cases.

If you compare the max Vio value between LM224 and LM224A you can see a difference of 2mV.

Ambient:5mV -> 3mV(A version)

Temperature:

7mV -> 5mV(A version)

Regards

Florian