Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

LMV321ILT 3.3V operational compatibility

Hi,@Peter BENSCH In the datasheet of ST LMV321ILT op-amp, it is stated that minimum voltage supply span is 2.7V and maximum supply span is 6V. Can you suggest whether LMV321ILT can be used with 3.3V or an alternate that is both pin to pin and 3.3V co...

I have conducted the double pulse test on the sct070h120g3ag SIC MOSFET . and I have compared the switching loss to the datasheet of the MOSFET. The Losses of the MOSFET is 3 times more than the loss on the Datasheet .

Could you advise me if there are an explanation of the energy loss seen on the Sic mounted on the PCB which is higher than the energy loss on the Datasheet .Thanks ,

MSIWA.1 by Associate
  • 3182 Views
  • 1 replies
  • 0 kudos

TDA7294 Spice Model

Hello,Is there a TDA7294 spice model? I am an engineering student doing my Bachelor's audio project and would help me in the development of the project.Best,João Santos

Resolved! Help identifying specific 2904

Need to replace this. I'm assuming the one on the left is toast just from a visual inspection. Can someone tell me which specific version I need to get? I'm not sure if the "EZ605" designator means anything. Any suggestions are appreciated. Thanks!  ...

2904.jpg

Resolved! Codec's channels

Hi, I hope finding an answer this is my first time asking you.  So, I'm trying to build a CLASS_D AMPLIFIER with codec (STA309A). This codec has 8 input channels for serial AUDIO and I want to play more channels for the codec's inputs but the I2S can...

Tom_Gean by Associate II
  • 14655 Views
  • 1 replies
  • 0 kudos

Resolved! Poblem with LM358DT and not with LM324AD

Dear all, the first of all thanks for let me leave a message in this post.We have a schematic circuit, with the LM324 it works but with the LM358 doesn´t work. It gives the correct voltage in both chips in the output, I connect a relay solid state fr...

DifferenceLM358-LM324.jpeg esquema.PNG

TDA7292 with Single Supply

Hi, I made a circuit for the TDA7292 with a simple power supply as shown in the brochure. The standby and off functions work well, but the low tones become distorted when I increase the volume more. The circuit works with 12VDC. Is it because more DC...

single_tda7292.png
Alanrav by Associate
  • 2077 Views
  • 1 replies
  • 1 kudos