Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

RHF1401 - Protection diodes for VIN and VINB

We use the RHF1401 in a space application. In front of the RHF1401 we have a single to differential buffer, which is susceptible for radiation transients. So it can occur, that the RHF1401 receives a transient with -1.3V to 5.55V at is inputs. The tr...

Figure3.png
ale-s by Associate
  • 2662 Views
  • 2 replies
  • 0 kudos

HELP! Echo cancellation - VoIP Solution - FP-AUD-AEC1

Hi everyone!I am working on a VoIP intercommunicator. The problem is that the audio coming from the microphone comes with echo. I am currently using a Raspberry PI 3 for running the SIP Client, but I am planning to use the FP-AUD-AEC1 function pack i...

grey1 by Associate
  • 1298 Views
  • 0 replies
  • 0 kudos

TSV912 MiniSO8 Footprint (Datasheet error?)

I am laying out a PCB and would like to use the TSV912IST, which has a MiniSO8 footprint. See page 18 of the datasheet linked on this page: https://www.st.com/en/automotive-analog-and-power/tsv912.html(DS4899 - Rev 12 - November 2019)I believe that t...

Newtham by Associate II
  • 3603 Views
  • 3 replies
  • 3 kudos

Resolved! TSU114: Dual Supplies and QFN-16 EP

Hello,I would like to use the TSU114 in the QFN-16 package and have 2 questions:1. Can the TSU11x be used with a dual supply?  For example, can I put +1.8V on VCC+ and -1.8V on VCC-?2. How should I connect the EP of the QFN-16 package?  The datasheet...

Spice model for STW12N170k5

Hi there,Can anyone direct me to a Spice model for the STW12N170k5 power MOSFET?I’m relatively new to using LTSpice so any guidance on how to apply a more precise model to the default M1 model would be appreciated.I attach the circuit so far (D1 is i...

How can i get the Vbat actual value from ADC?

Hello,i'm using STM32G070, The firmware i have programmed converts the analog voltage to didital using ADC. the code is below:the values i get from this is :OUTPUT:In the datasheet it is mention that a resister bridge for VBAT is 39K ohm which has ra...

_legacyfs_online_stmicro_images_0693W00000dDX43QAG.png _legacyfs_online_stmicro_images_0693W00000dDX48QAG.png _legacyfs_online_stmicro_images_0693W00000dDX4IQAW.png
MQasi.2 by Associate II
  • 3543 Views
  • 2 replies
  • 0 kudos

Resolved! SPICE Model for TS912BIDT

Hi! I need a SPICE model for TS912BIDT. I couldn't find it anywhere. Please help! Thank You!

Vishakha by Associate II
  • 3141 Views
  • 2 replies
  • 2 kudos

Resolved! G Letter on TDA7297

Hi, everyoneWhat does the letter G printed on the STmicroelectronics TDA7297 IC mean?See attached image fileThanks

G on TDA7297.jpg

Resolved! TSV912IQ2T absolute maximum input voltage

The following are some questions related to the absolute maximum ratings of the TSV912IQ2T which are not clear from the datasheet. Can the voltage on the input pins (2,3,5 and 6) swing to values greater than VCC + 0.2V (for example 50V) if the curren...

whabib by Associate
  • 2395 Views
  • 1 replies
  • 1 kudos