2024-09-24 03:50 PM
Hello,
I would like to use the TSU114 in the QFN-16 package and have 2 questions:
1. Can the TSU11x be used with a dual supply? For example, can I put +1.8V on VCC+ and -1.8V on VCC-?
2. How should I connect the EP of the QFN-16 package? The datasheet mentions that the EP of the DFN-8 package should be connected to VCC- or left floating, but doesn't say how the EP of the QFN package should be connected.
Thank you for any guidance you can provide.
Michael
2024-09-26 04:05 AM
Welcome @michael-imagia, to the community!
Hope that helps?
Regards
/Peter