WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Most recent activity
Hello,We are designing a custom board using the STM32MP157FAC1 device and need to provide provision for a Serial NOR Flash connected to the QUADSPI interface.We are planning to use Winbond's device W25Q256JVFIQ for this purpose. Kindly confirm whether this device is suitable for use with the STM32MP157FAC1 or if there is any recommended QSPI NOR Flash device that should be preferred with this microprocessor.Regards,Prashant
Hi!My Linux is booting on my custom board. This board is using 2 GB (16-bit density) instead of 4 GB (32-bit density).So, when Linux is booted. I get this.Can it be so CubeMX is only fixed to 4GB when selecting STM32MP257F? Any suggestions? The complete log is attached.I'm using USART6 as debugging tool. flags=600, drv->flags=0, err=-129 Sending event 6/(unknown) to spy 'efi_disk del' Sending event 6/(unknown) to spy 'efi_disk del' eth1_clk_mx-0: When removing: flags=600, drv->flags=0, err=-129 Sending event 6/(unknown) to spy 'efi_disk del' eth1_mdio_mx-0: When removing: flags=600, drv->flags=0, err=-129 Sending event 6/(unknown) to spy 'efi_disk del' eth1_rgmii_mx-0: When removing: flags=600, drv->flags=0, err=-129 Sending event 6/(unknown) to spy 'efi_disk del' sdmmc1_mx-0: When removing: flags=600, drv->flags=0, err=-129 Sending event 6/(unknown) to spy 'efi_disk del' usart6_mx-0: When removing: flags=600, drv->flags=0, err=-129 pinctrl@44240000: When re
I’m reading the getting started manual of STM32MP257 (AN5489) and it displays that there are internal pull-ups on CMD and D0, but not CK.Also there is a confusion if the dashed lines means they have internal pull-ups as well.My question is:If CMD, D0, D1, D2 and D3 have internal pull-ups. Why does the STM32MP257F-DK board have external pull-ups?Can I skip these external pull-ups? According to the datasheet of STM32MP257C/F (DS14284 - Rev 5), the CK, CMD and D0 MUST be high at initialisation of the BootROM.
Hello ST Team,I am evaluating the STM32MP215F-DK with the recommended M.2 Wi-Fi/BT module (Embedded Artists EAR00409 / Murata 2EL). I have encountered two critical issues that prevent the Wi-Fi features from working out-of-the-box with the standard Starter Package.I believe these are bugs in the current hardware/software release.1. Critical Software Configuration Issue: SDMMC2 Access Blocked by RIFThe STM32MP215F-DK Data Brief explicitly states that the board features an "M.2 E-Key connector to support Wi-Fi® and Bluetooth® SDIO modules". However, with the default Starter Package (OpenSTLinux 6.6), the Linux kernel fails to probe the Wi-Fi module on SDMMC2.Symptoms:• Linux kernel log shows no response from mmc1 (SDMMC2).• Attempting to access the SDMMC2 registers manually via devmem 0x48230000 results in a Bus Error.• OP-TEE console reports a firewall exception: SERC exception ID: 77 (SDMMC2 Illegal Access).Root Cause Analysis: It appears that the Trusted Firmware-A (TF-A) device tree
Hello,I am working on the STM32MP257F-DK board and would like to use two Ethernet interfaces simultaneously for industrial network communication.The board provides:One onboard RJ45 Ethernet connector. One USB Type-C connector that, according to the documentation, can also provide Ethernet connectivity.My objective is to establish a network ring topology, where both Ethernet interfaces are connected to external devices using RJ45 Ethernet cables.I would like to understand:How can the USB Type-C Ethernet interface be converted to a standard RJ45 Ethernet connection? Does the USB Type-C port support Ethernet through a USB-to-Ethernet adapter (USB Ethernet dongle)? If yes, are there any ST-recommended USB-to-RJ45 adapters that have been validated with STM32MP257F-DK? Under Linux/OpenSTLinux, will the onboard RJ45 and the USB Ethernet adapter appear as two independent network interfaces (for example eth0 and eth1)? Has anyone implemented Ethernet ring topologies such as MRP, RSTP, PRP, or c
Hello Support Team,I am trying to start SWD debugging for the STM32MP135DAF7 in STM32CubeIDE using an ST-LINK V2 probe, but I cannot get the debugger to work correctly.My development board is MYD-YF135-256N256D-100-I based on STM32MP135DAF7.I enabled Engineering boot mode (B2 = 1, B1 = 0, B0 = 0)Software versions:STM32CubeMX v6.17.0STM32CubeIDE v2.1.1STM32CubeMP13 Firmware Package V1.2.0Debugger:Original ST-LINK V2Serial number: 30FF6F064E58373521xxxx43Firmware version: V2J47S7I created a simple project in STM32CubeMX and enabled only RCC and SWD debug. Then I opened the project in STM32CubeIDE and configured debugging through OpenOCD with “Connect under reset”.The debugger can detect the target correctly:SWD DPIDR is detectedCPU examination succeedsThe core sometimes halts correctlyBut after that, the debug session fails with many OpenOCD errors such as:timeout waiting for DSCR bit changeError waiting for InstrCompl=1Error waiting for cortex_a_exec_opcodeFail reading CT
Can the clkout clock on the PHY chip be disabled, and how is it configured?
On the STM32MP135F-DK, is the 4.3" LCD module physically removable? Or is CN16 accessible without removing the LCD?
Hello ST community,I’m an embedded software beginner working with the STM32MP257-DK board and OpenSTLinux (Yocto). I need help getting USART6 working on the external GPIO connector (PF13 = TX, PF14 = RX — CN5 pins). I have rebuilt device trees and copied DTBs to the board, but the USART6 device never appears in the running system (/dev/ttySTM6), and at one point my Ethernet/SSH stopped working after applying a DTB change.I will be blunt: I have spent many hours following suggestions, debugging, and fixing syntax errors in DTS files. I may be missing one critical detail about how ST maps peripherals on the DK board or about kernel bindings. I have documented exactly what I tried and the exact outputs — please read fully before replying. I am a beginner; please do not assume I know advanced DT or U-Boot internals.Environment / versionsBoard: STMicroelectronics STM32MP257F-DK (discovery/“DK” board)Host SDK: SDK-x86_64-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11Kernel source / s
Hello,I'm working with the STM32MP135F-DK kit and I'm trying to understand the correct way to configure interrupt lines (IRQs) for external devices, specifically for the STPMIC1 in OP-TEE.I have been reading the official documentation and I'm a bit confused about whether it is mandatory to use the dedicated PWR Wake-up pins (WKUP1–WKUP6) for interrupt lines, or if any GPIO can be used.--- What I observed in the reference DTS files: Looking at the OP-TEE device tree (core/arch/arm/dts/stm32mp135f-dk.dts, tag 4.0.0-stm32mp), I can see that all IRQ consumers use EXTI lines above 55: - STPMIC1 interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING> (WKUP1 / PF8) --- My questionsIs it mandatory to use one of the 6 dedicated WKUP pins (EXTI 55–60) for any device IRQ managed by OP-TEE?
I'm using the mp215 with ddr3l (x16) and an ISSI dram ic that is 8Gb (1 gigabyte) which means it's a dual rank configuration compared to a more typical half gigabyte. As far as im aware all 1GB ddr3 dram ic's are dual rank.In AN5723 6.1 Note it says "8 Gbit DDR3 defined by JEDEC is uncommon. Practically, DDR3L density is limited to 4 Gbits (max = 1 Gbyte in total). Single rank only is required. ".an5723 link As far as I understand it it says it's not possible. However this is an older AN and i think it's for the mp25 series only (im using the mp21).However in the ST Wiki "How to setup the DDR configuration" section 5 the exact opposite is implied. This whole section repeatedly describes a "concrete example" of swapping the swapping the mp215-dk's lpddr4 out with a 1GB ddr3 ic. Also using a theoretical dtsi called "stm32mp21-ddr3-1x8Gbits-1x16bits-800MHz.dtsi" and define "DDR_MEM_SIZE 0x40000000" which is 1GB. So this is conflicting info because i dont see how 1gb ddr3 is poss
Hi~ My board gets stuck at the kernel stage during boot. I've referred to numerous related posts but failed to resolve the issue.The boot file versions I use are OP-TEE 4.0, U-Boot 2023.10 and Linux 6.6.116.The official device tree I referenced is stm32mp157f-ed1.I have attached the boot logs, hardware schematic and device tree files. Please help analyze the root cause of the problem. stm32f7-i2c i2c@5c002000: pinctrl_select_state_full: pinctrl_config_one: err=-19 [ 1.741795] arm-scmi firmware:scmi: SCMI Protocol v2.0 'ST:' Firmware version 0x0 [ 1.748959] DEBUG: SCMI CLOCK PROBE STARTED! sdev name: scmi_dev.2 I/TC: SCMI-CLOCK: Reporting 34 clocks to Linux I/TC: SCMI-FW: ETZPC ID 2 DENIED for Non-Secure world! I/TC: SCMI-MSG: NS Request Clock ID 15 (iwdg1), ETZPC 2, Access=FAIL I/TC: SCMI-CLK: ID 15 has no name/not found I/TC: SCMI-FW: ETZPC ID 7 DENIED for Non-Secure world! I/TC: SCMI-MSG: NS Request Clock ID 16 (rng1_k), ETZPC 7, Access=
Hello all,We are bringing up DDR4 memory on a custom STM32MP257D-based SOM. We have made significant progress but are now blocked on a specific PHY training failure that we cannot diagnose without access to the Synopsys PHY firmware streaming message documentation. We would appreciate any help interpreting the failure and identifying the root cause.Board OverviewSoC: STM32MP257DAK3 (VFBGA424)DRAM: 2× Alliance AS4C512M16D4A-62BIN (DDR4-3200, 8 Gbit × 16, 1.2V, VPP 2.5V)Topology: 32-bit bus, 2 GB total, single rank, soldered downPMIC: STPMIC25APQR (I²C7)Reference HSE: 40 MHz crystalTool chain: STM32CubeMX 6.16.1, STM32CubeIDE 2.0.0, STM32DDRFW-UTIL, STM32CubeProgrammer 2.22Bring-up StatusWe are using STM32DDRFW-UTIL with verbose PHY messaging enabled (hdtctrl = 0x05, custom g_waitfwdone.c patched to decode major messages and dump streaming messages).Power Rails (all verified by HW measurement)VDD_DDR: 1.20 V :white_heavy_check_mark:VTT_DDR: 0.60 V :white_heavy_check_mark:VREF_DDR: 0.60 V
Hello,I have been trying for some time now to connect a Raspberry Pi 7" screen to my STM32MP157F development kit, as the screen that comes with it is too small for my purposes. I do not have a large amount of experience with embedded systems or working at the Linux kernel level. I have been referencing the display wiki page, however I have not been able to get the screen to output anything, only for the backlight to turn on. I have been plugging in the 15 pin connector into the 20 pin CN4 port on the board, which is stated to work on the wiki. I have seen this adapter referenced online, but I would rather not have to order it if not necessary as I am on a time crunch. I have tried many different device tree configurations, in addition to the example given on the wiki. I am at a loss here, and would greatly appreciate any guidance. Below is snippet from my device tree, which I have modified from the wiki. &dsi { status = "okay"; ports { port@0 { reg = &
Hi all,I have a board designed around the STM32MP153FAD (TFBGA257, 10×10 mm, 0.5/0.65 mm pitch, 257 balls). Since the MP153 does not include a DSI controller or GPU, I did not connect any DSI-related power pins or signals. Due to stock shortages, I am now considering switching to the STM32MP157FAD, which shares the same TFBGA257 footprint.My question is: can the STM32MP157FAD be used on this board without connecting the DSI-specific power rails?The DSI power pins that exist on the MP157 but were not populated on my design are:VDD_DSI — DSI I/O supplyVDD1V2_DSI_REG — output of internal 1.2 V DSI regulatorVDD1V2_DSI_PHY — 1.2 V supply for DSI PHYVDDA1V8_DSI — 1.8 V analog supply for DSIMy concern is whether the MP157 will operate correctly (for non-DSI use cases) if these pins receive no supply. (Unused pins are floating right now, is that correct or should I connect it to GND)I have attached my current schematic for reference.Any guidance would be appreciated.Best regardsRegards
I'm working on STM32mp25f-EV1, i have downloaded FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18 package but i'm facing problem while accessing SSH.
Hi,I am working on STM32MP135 with SGTL5000 codec using ALSA/ASoC.Playback is working correctly:aplay -D default /home/audio/test_audio.wavBut audio capture is failing with Input/output error:root@stm32mp135-comtrol:~# arecord -D hw:0,1 -f S16_LE -r 48000 -c 2 test.wav Recording WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo arecord: pcm_read:2272: read error: Input/output errorCurrent status:Playback works correctlyCodec detected properlyI2C communication seems OK during playbackCapture stream fails immediately after startroot@stm32mp135-comtrol:~# arecord -l **** List of CAPTURE Hardware Devices **** card 0: STM32SGTL5000 [STM32-SGTL5000], device 1: 4400a024.audio-controller-sgtl5000 sgtl5000-1 [4400a024.audio-controller-sgtl5000 sgtl5000-1] Subdevices: 1/1 Subdevice #0: subdevice #0 Device tree configuration is attached below.Questions:What usually causes pcm_read: Input/output error in ALSA capture?Could this be related to SAI RX configuration?Is there
Hello,For students, we recently bought the STM32MP257F eval board, and the related camera and hdmi bridge.Everything works perfectly and I would like to connect a Raspberry Camera v2. (IMX219) to the board, as it is also a CSI/MIPI camera (and whe have severals).Can it work ? what should be done related to the software ? (drivers and so on).By the way, what is the process to install packages in the board ?Best regardsS. M.
Hi!I have a custom board with 2GB RAM instead of 4GB RAM. Yes, I have configured 2GB in CubeMX and generated the new DT.Check it out here: https://github.com/DanielMartensson/Watermelon-Wine-1A/tree/linux-testing/watermelon-wine-os%2Flayers%2Fmeta-watermelon-wine%2Fmx%2Fwatermelon-wine-1aIt seems that the booting process passes TF-A without any issues. But it fails at the optee boot process.F/TC:0 0 regulator_enable:94 v3v3 F/TC:0 0 regulator_enable:94 v5v_vconn [ 0.000000] SCP-firmware 2.13.0-intree-optee-os-4.0.0-dev [ 0.000000] [ 0.000000] [FWK] Module initialization complete! F/TC:0 0 regulator_set_voltage:202 vddcpu 800000uV F/TC:0 0 lock_i2c_bus_access:796 thread access F/TC:0 0 unlock_i2c_bus_access:837 thread access completed F/TC:0 0 stpmic2_register_read:259 REG[0x20 v=0x1e F/TC:0 0 pmic_get_voltage:192 vddcpu: get voltage: 800000 uV F/TC:0 0 pwr_get_state:243 vddgpu: get state D/TC:0 0 set_opp:60 set volt to 800000uV F/TC:0 0 regulator_set_voltage:202 vddgpu 800000uV F/T
Hi, I'm new to yocto project, I'm trying to bitbake core-image-minimal image in yocto in stm32mp157d-dk1(scarthgap) ,by editing the bblayers.conf and local.conf in image, its successfully build and flashed into SD card , but I'm trying to boot device then it failed. I found in bootfs sector there was no files in it. I tried to build with kirkstone branch and it worked well, and then I tried to bitbake with scarthgap again and again. I used Ubuntu 24.04 and Linux mint 22.03, but scarthgap branch had the same problems.I wanna know the reason. BIG THX.
Hi,I'm using brand-new, unmodified st32mp257f-dk dev board.When using starter package (https://www.st.com/en/embedded-software/stm32mp2starter.html#get-software) flashed onto sdcard according to https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command, system boots-up fine, see 'downloaded_no_panic.log'. Version is openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.When using image built on my own - distribution package (openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11) according to https://wiki.st.com/stm32mpu/wiki/STM32MPU_Distribution_Package, using docker, I get following:[ 8.296788] usb 1-1: new high-speed USB device number 2 using ehci-platform [ OK ] Found device /dev/hwrng. [ OK ] Found device /dev/tee0. [ 9.041963] hub 1-1:1.0: USB hub found E/TC:0 0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r2/core/drivers/clk/clk-stm32mp25.c:2000 <clk_stm32_pll_init> [ 9.142742] hub 1-1:1.0: 2 ports detected E/TC:0 0 TEE load ad
Hi, Just now I have done bringing up a custom board for STM32MP133/ STM32MP135 with OpenST Linux, with kernel 6.2:- The whole boot chain bring up from tf-a, uboot, kernel.- Configure PMIC and support DDR test.- Support FMC NAND, change flash partition layout.- A/B FOTA ready Yocto build (with uboot)- Total boot time is 30 seconds to access to ADB (android platform tool)- Platform CAN bringup- Integrate Quectel modem for network over LTEIf someone needs something related to this, I can help.Best,Eric
Hi,this one is similar to https://community.st.com/t5/stm32-mcus-products/ioselect-option-in-stm32h563-is-not-working/m-p/681099but not the same. While testing OSPI1 on our MP257 board and our FSBL I found thatMSEL in OCTOSPI1->CR is ignored.CSSEL and DMM are honored and works as expected but when DMM=0 then output signalsare the same on both IO[3:0] and IO[7:4].Attached is analyzer output of CLK,CS,IO0,IO4 for transaction with relevant regs:0x50430000: 00000f010x50430100: 04002101AR was 0xfa0000 and 8 bytes was sent to DR.Martin
Is there a Global Exclusive Monitor connected to the M33 and the A35 cores?Any documentation for it?Thank you
We have some devices based on STM32MP257 SoCs that connect to a 100 Mbit Ethernet network via ETH1, where ETH1 is going straight to an RMII PHY. Pins for ETH2 are reserved, but are not used/not connected. Some of our devices work rock-solid as excepted, but others exhibit massive performance problems on the Ethernet connection.After lots of research, we think that our devices are affected by a silicon bug described in errata sheet ES ES0598 as "ETH1 RMII mode could have CRC errors". Our chip revisions are all rev Y, which are affected by the issue. The errata says that ETH1 should be routed through ETHSW to work around the silicon bug. To test if the workaround works for our case, I've tried to enable ETHSW, but failed so far because STM32CubeMX forces me to free some pins before it allows me to enable ETHSW in RMII mode. It seems like ETH1 and ETH3 must be used together if ETHSW is enabled, the pins for ETH3, however, are already used for other hardware functions.So, my goal is to- en
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.