Skip to main content
Visitor II
Feb 7, 2025 1:49 PM UTC
Question

STM32MP257F & Raspberry Camera v2. (IMX219)

Hello,

For students, we recently bought the STM32MP257F eval board, and the related camera and hdmi bridge.

Everything works perfectly and I would like to connect a Raspberry Camera v2. (IMX219) to the board, as it is also a CSI/MIPI camera (and whe have severals).

Can it work ? what should be done related to the software ? (drivers and so on).

By the way, what is the process to install packages in the board  ?

Best regards

S. M.

 

 

1 reply

Associate II
May 14, 2026 2:53 AM UTC

Hello,

I also use Raspberry Camera v2. (IMX219) porting on STM32MP257F MPU.

I doubt whether this camera module is compatible with STM32MP257.

This camera can support 8M pixel, but STM32MP257 only support 5M pixel.

Does any one can help me?