Skip to main content
Marzarsh
Associate
May 1, 2026 5:51 PM UTC
Question

STM32MP157D-DK1 yocto build problem of scarthgap problem

Hi, I'm new to yocto project, I'm trying to bitbake  core-image-minimal image in yocto in stm32mp157d-dk1(scarthgap) ,by editing the bblayers.conf and local.conf in image, its successfully build and flashed into SD card , but I'm trying to boot device then it failed. I found in bootfs sector there was no files in it. I tried to build with kirkstone branch and it worked well, and then I tried to bitbake with scarthgap again and again. I used Ubuntu 24.04 and Linux mint 22.03, but scarthgap branch had the same problems.I wanna know the reason. BIG THX.

6 replies

Marzarsh
MarzarshAuthor
Associate
May 1, 2026 5:56 PM UTC

Marzarsh_0-1777658153867.png

my bblayers file

Visitor II
May 7, 2026 6:57 PM UTC

I have also built core-image-minimal according to the instructions and without making any changes at all to the default files, and I’m getting exactly the same error as you: no files in boot partition. I’ve tested on both boards 215F-DK and 257F-DK, and flashed using STM32_Programmer_CLI and raw mode. I’ve also tried many different TSV files, but nothing helps. So it seems to be a general issue in the Distribution-Package build environment.
I’d appreciate it if anyone has a suggestion for a solution.

Marzarsh
MarzarshAuthor
Associate
May 8, 2026 1:08 AM UTC

Use kirkstone branch will solve this problem but it is not newest branch.

Visitor II
May 7, 2026 7:08 PM UTC

Here is my boot log:

STM32MP> NOTICE: CPU: STM32MP215FAN Rev.Z
NOTICE: Model: STMicroelectronics STM32MP215F-DK Discovery Board
NOTICE: Board: MB2059 Var1.0 Rev.B-02
NOTICE: Reset reason: Pin reset from NRST (0x2034)
INFO: PMIC2 version = 0x12
INFO: PMIC2 product ID = 0x31
INFO: FCONF: Reading TB_FW firmware configuration file from: 0xe011000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp2-r2.0(debug):lts-v2.10.24-dirty(a07367a1)
NOTICE: BL2: Built : 16:16:36, Oct 3 2025
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0xe061000
INFO: Image id=26 loaded: 0xe061000 - 0xe069650
INFO: BL2: Doing platform setup
INFO: RAM: LPDDR4 1x16Gbits 1x16bits 800MHz
INFO: Memory size = 0x80000000 (2048 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0xe000000
INFO: Image id=1 loaded: 0xe000000 - 0xe000326
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0xe000000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: risaf_config
INFO: RISAF2: No configuration in DT, use default
INFO: BL31 max size = 0x17000 (94208B)
INFO: BL2: Loading image id 3
INFO: Loading image id=3 at address 0xe000000
INFO: Image id=3 loaded: 0xe000000 - 0xe015978
INFO: BL2: Loading image id 19
INFO: Loading image id=19 at address 0x81fc0000
INFO: Image id=19 loaded: 0x81fc0000 - 0x81fc330a
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x82000000
INFO: Image id=4 loaded: 0x82000000 - 0x8200001c
INFO: OPTEE ep=0x82000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x1
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x82000000
INFO: Image id=8 loaded: 0x82000000 - 0x820fa008
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0x84400000
INFO: Image id=2 loaded: 0x84400000 - 0x84416470
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0x84000000
INFO: Image id=5 loaded: 0x84000000 - 0x841b3600
NOTICE: BL2: Booting BL31
INFO: Entry point address = 0xe000000
INFO: SPSR = 0x3cd
INFO: ARM GICv2 driver initialized
NOTICE: BL31: v2.10-stm32mp2-r2.0(debug):lts-v2.10.24-dirty(a07367a1)
NOTICE: BL31: Built : 16:16:36, Oct 3 2025
INFO: BL31: Initializing runtime services
INFO: BL31: Initializing BL32
I/TC: Early console on UART#2
I/TC:
I/TC: Embedded DTB found
I/TC: OP-TEE version: 4.0.0-dev (gcc version 13.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: WARNING: All debug access are allowed
I/TC: Override the OTP 124: 0 to 0x8db6
I/TC: WARNING: Embeds insecure stm32mp_provisioning driver
I/TC: PMIC STPMIC REFID:3.A V1.2
I/TC: Platform stm32mp2: flavor PLATFORM_FLAVOR - DT stm32mp215f-dk.dts
I/TC: OP-TEE ST profile: secure_and_system_services
I/TC: DBGMCU Authenticated Debug Mailbox online
[ 0.000000] SCP-firmware 2.13.0-intree-optee-os-4.0.0-dev
[ 0.000000]
[ 0.000000] [FWK] Module initialization complete!
I/TC: Primary CPU switching to normal world boot
INFO: BL31: Preparing for EL3 exit to normal world
INFO: Entry point address = 0x84000000
INFO: SPSR = 0x3c9
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are enabled


U-Boot 2023.10-stm32mp-r3 (Oct 02 2023 - 14:39:59 +0000)

CPU: STM32MP215FAN Rev.Z
Model: STMicroelectronics STM32MP215F-DK Discovery Board
Board: stm32mp2 (st,stm32mp215f-dk)
Board: MB2059 Var1.0 Rev.B-02
DRAM: 2 GiB
optee optee: OP-TEE: revision 4.0 (2a5b1d12)
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are enabled
Core: 322 devices, 37 uclasses, devicetree: board
WDT: Started watchdog with servicing every 1000ms (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
Net: eth0: eth1@482c0000
No EFI system partition
No EFI system partition
Failed to persist EFI variables
Hit any key to stop autoboot: 0
Boot over mmc0!
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:8...
BootOrder not defined
EFI boot manager: Cannot load any image
STM32MP> ext4ls mmc 0:8 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
STM32MP>