Skip to main content
AVazquez
Associate III
May 15, 2026 2:55 PM UTC
Solved

[STM32MP135F-DK] STPMIC1 IRQ in OP-TEE Can I use a non-WKUP GPIO?

Hello,

I'm working with the STM32MP135F-DK kit and I'm trying to understand the correct way to configure interrupt lines (IRQs) for external devices,  specifically for the STPMIC1 in OP-TEE.

I have been reading the official documentation and I'm a bit confused about whether it is mandatory to use the dedicated PWR Wake-up pins (WKUP1–WKUP6) for interrupt lines, or if any GPIO can be used.

---

What I observed in the reference DTS files:

Looking at the OP-TEE device tree (core/arch/arm/dts/stm32mp135f-dk.dts, tag 4.0.0-stm32mp),

I can see that all IRQ consumers use EXTI lines above 55:

- STPMIC1 interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING> (WKUP1 / PF8)

---

My questions

Is it mandatory to use one of the 6 dedicated WKUP pins (EXTI 55–60) for any device IRQ managed by OP-TEE?

 

ZAKARIA_C1Best answer
ST Employee
Jun 9, 2026 2:13 PM UTC

Hello ​@AVazquez,
 

  • No, it is not mandatory to use WKUP1–WKUP6 (EXTI 55–60) for all external device IRQs in OP-TEE.

  • WKUP pins are special:

    • Used for wake-up from Standby when PWR is assigned to OP-TEE.

    • Must be configured in &pwr_irq with wakeup-gpios.

  • Other GPIOs (EXTI 0–54):

    • Can be used as normal interrupt sources.

    • Set up via stm32-irq-notifier and forwarded to Linux via OP-TEE notifications.

  • For STPMIC1 on STM32MP135F-DK, using WKUP1 is chosen because the PMIC manages power and wake-up, not because it's mandatory for all devices.


Best Regards,
Zakaria

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

ZAKARIA_C1Best answer
ST Employee
Jun 9, 2026 2:13 PM UTC

Hello ​@AVazquez,
 

  • No, it is not mandatory to use WKUP1–WKUP6 (EXTI 55–60) for all external device IRQs in OP-TEE.

  • WKUP pins are special:

    • Used for wake-up from Standby when PWR is assigned to OP-TEE.

    • Must be configured in &pwr_irq with wakeup-gpios.

  • Other GPIOs (EXTI 0–54):

    • Can be used as normal interrupt sources.

    • Set up via stm32-irq-notifier and forwarded to Linux via OP-TEE notifications.

  • For STPMIC1 on STM32MP135F-DK, using WKUP1 is chosen because the PMIC manages power and wake-up, not because it's mandatory for all devices.


Best Regards,
Zakaria

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.