Skip to main content
Associate II
Apr 9, 2026 10:45 PM UTC
Question

STM32MP135F-DK, is the 4.3" LCD module physically removable?

On the STM32MP135F-DK, is the 4.3" LCD module physically removable? Or is CN16 accessible without removing the LCD?

2 replies

Olivier GALLIEN
ST Technical Moderator
Jun 11, 2026 9:41 AM UTC

Hi ​@Jled,

Yes, indeed maybe not that simple but Ok. 

By curiosity what do you plan to do ? 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JledAuthor
Associate II
Jun 11, 2026 9:49 AM UTC

Hi ​@Jled,

Yes, indeed maybe not that simple but Ok. 

By curiosity what do you plan to do ? 

Olivier 

Hi Oliver, this is a test unit along with the MP257 DK board. I am going to output to multiple screens and also output formats like composite, LDVS, and others. I will then design a custom mp2 powered board with multiple output options.