Skip to main content
MC.4
Associate II
June 30, 2022
Question

I2C master transmit and slave receive functions work. Master receive and slave transmit don't.

//MASTER
while (1)
 {
 /* USER CODE END WHILE */
 
	 ret = HAL_I2C_Master_Transmit(&hi2c1, peripheralNucleoAddress << 1, bufferTx, 1, HAL_MAX_DELAY);
	 if (ret != HAL_OK)
	 {
		 strcpy((char*) bufferTx, "Tx");
		 HAL_UART_Transmit(&huart2, bufferTx, strlen((char*) bufferTx), 1000);
		 HAL_Delay(500);
		 //Error_Handler();
	 }
 
 
	 
	 ret = HAL_I2C_Master_Receive(&hi2c1, peripheralNucleoAddress << 1, bufferRx, 1, 1000);
	 if (ret != HAL_OK)
	 {
		 strcpy((char*) bufferRx, "Rx");
		 HAL_UART_Transmit(&huart2, bufferRx, strlen((char*) bufferRx), 1000);
		 HAL_Delay(500);
		 //Error_Handler();
	 }
 
 
 /* USER CODE BEGIN 3 */
 }
 
 
---------------SEPARATE FILE----------------------------------------------------------------------------
 
 
//SLAVE
 while (1)
 {
 
 /* USER CODE END WHILE */
	 ret = HAL_I2C_Slave_Receive(&hi2c1, bufferRx, 1, HAL_MAX_DELAY);
 
	 if (ret != HAL_OK)
	 {
		uint8_t message[9];
		strcpy((char*) message, "Fail RX!");
		HAL_UART_Transmit(&huart2, message, strlen((char*) message), 5000);
		//Error_Handler();
	 }
 
	 if (bufferRx[0] == 0x00)
	 {
		uint8_t message[16];
		strcpy((char*) message, "Buffer is zero!");
		HAL_UART_Transmit(&huart2, message, strlen((char*) message), 5000);
		//Error_Handler();
	 }
 
	 else if (bufferRx[0] == 0xAA)
	 {
		uint8_t message[16];
		strcpy((char*) message, "Buffer is 0xAA!");
		HAL_UART_Transmit(&huart2, message, strlen((char*) message), 5000);
		//Error_Handler();
	 }
 
	 else if (bufferRx[0] == 0xFF)
	 {
		uint8_t message[16];
		strcpy((char*) message, "Buffer is 0xFF!");
		HAL_UART_Transmit(&huart2, message, strlen((char*) message), 5000);
		//Error_Handler();
	 }
 
 
	 ret = HAL_I2C_Slave_Transmit(&hi2c1, bufferTx,1, 1000);
	 if (ret != HAL_OK)
	 {
		uint8_t message[9];
		strcpy((char*) message, "Fail TX!");
		HAL_UART_Transmit(&huart2, message, strlen((char*) message), 5000);
		//Error_Handler();
	 }
 
 
 
	 HAL_Delay(500);
 /* USER CODE BEGIN 3 */
 }

I am using two NucleoG071 boards to create an I2C communication, in which one acts as the master and the other as the slave. For some reason the I2C master receive function and slave transmit do not work even though the master transmit and slave receive do. Any tips are highly appreciated.

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
June 30, 2022

"Any tips are highly appreciated"

As I said in your previous thread, the Key Tip: Don't try to implement both ends of the link at once!

https://community.st.com/s/question/0D53W00001ddlCxSAI/connecting-two-nucleo-boards-using-i2c

Otherwise, you have too many unknowns - when something doesn't work, you can't tell if it's because

  • the master is wrong/broken
  • the slave is wrong/broken
  • both are wrong/broken
  • other things are wrong/broken...

Concentrate on getting just one end working & thoroughly debugged - using a known-good standard implementation at the other end.

Again, see: https://www.avrfreaks.net/comment/2320631#comment-2320631

The other key tip: This is not just a software problem - you also need to be looking at the wires with an oscilloscope and/or analyser to see what's actually happening in the hardware.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MC.4
MC.4Author
Associate II
June 30, 2022

So after I couldn't make it work like that I did end up following your tip from my previous post and tried making only the Master Receive work. However, I still had no luck as my clock line for some reason gets pulled low when I add a second board even though I am using pull up resistors.

When I try using the Master board by itself the clock and read and write requests work as well (though they don't get acknowledged since there is only one board connected).

To look at what's happening I am currently using the terminal for printing and a Logic Analyzer.

Andrew Neil
Super User
June 30, 2022

What "second board" ?

Have you tested your Master with a known-good, simple slave - like some standard, well-known I2C chip?

At this stage, an oscilloscope is probably better, as you can see any analogue nasties - such as wrong pullup values.

By putting a resistor in series with the lines, you can see which end is doing the pulling-down ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
July 1, 2022

"an oscilloscope is probably better, as you can see any analogue nasties - such as wrong pullup values"

For example: 

0693W00000Nt1crQAB.pnghttps://electronics.stackexchange.com/questions/1849/is-there-a-correct-resistance-value-for-i2c-pull-up-resistors

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.