VCO frequency discrepancy in STM32H743 datasheet and reference manuals
There is a discrepancy between rev 8 of the datasheet and rev 7 of the reference manual regarding the PLL VCO output range parameter when the PLL is setup in wide VCO frequency mode.
In section 7.3.10 of the datasheet, the VCO output range is between 192 and 960 MHz.
In section 8.7.12 of the reference manual, the documentation regarding the VCC#VCOSEL bits in the RCC_PLLCFGR register specifies a VCO output range is between 192 and 836 MHz.
I am pretty sure that the datasheet description is correct as I haven't encountered any issues configuring the micro with a 960 MHz VCO output, but would like an ST representative to confirm that and an assurance that the reference manual will be amended in future revisions.
Cheers,
Craig