How to on STM32Cube_FW_WL_V1.1.0
Hello,
I’m working with NUCLEO-WL55JC1. I’ve done some tests with STM32CubeIDE ver 1.6.1 firmware 1.0.0 (STM32Cube_FW_WL_V1.0.0) and, after some difficulty, it’s working as aspected. To fix ideas on the job done, I’ve made a Youtube video (https://youtu.be/40wuXKoA44Y).
Then I’ve updated STM32CubeIDE to version 1.7.0 and loaded a new firmware version 1.1.0. Of course, something is changed.
Now seems that the use of BSP Driver is mandatory (file platform.h row 32). I’ve imported in my project, from firmware 1.1.0, the BSP driver and added the path on the IDE setting.
Then I was able to compile without errors. I’ve sent the new code on the Nucleo board. It starts and I’ve initial data on debugger console. The initial try to connect to the TTN application shows that the join seems accepted, but then no more data are sent. It looks like if the loop (with default 1000 mS) does not take place. At the moment I have no idea how to proceed (again, I'll have to spend a very long time e to fix the problem :confounded_face: :) )
Can I have some help,
Thanks, Fabrizio