Skip to main content
DAlek
Associate II
June 16, 2021
Question

How to update STM32WB55CE FUS and wireless stack ?

Having issues with STM32WB55CE FUS and wireless stack update. FUS version:

Reading 32-bit memory content

Size : 4 Bytes

Address: : 0x20010010

0x20010010 : 01010100

FUS upgrade >STM32_Programmer_CLI.exe -c port=swd mode=UR -fwupgrade stm32wb5x_FUS_fw.bin 0x0807A000 firstinstall=0, getting:

Error: Could not execute fwupgrade command, Impossible to install FUS V1.0.1 on

256/512KB Flash Parts

Wireless stack update >STM32_Programmer_CLI.exe -c port=swd mode=UR -fwupgrade STM32WB55\stm32wb5x_BLE_Stack_full_fw.bin 0x08056000 firstinstall=0

-------------------------------------------------------------------

STM32CubeProgrammer v2.7.0

-------------------------------------------------------------------

ST-LINK SN : 52FF74067575555041500481

ST-LINK FW : V2J37S7

Board : --

Voltage : 3.26V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x495

Revision ID : Rev Y

Device name : STM32WB5x

Flash size : 512 KBytes

Device type : MCU

Device CPU : Cortex-M4

Old wireless stack delete ...

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

File : 0x495_FUS_Operator.bin

Size : 8 KBytes

Address : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.765

Application is running, Please Hold on...

Reconnecting...

Reconnected !

Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !

Firmware delete Success

Download firmware image at address 0x8056000 ...

Memory Programming ...

Opening and parsing file: stm32wb5x_BLE_Stack_full_fw.bin

File : stm32wb5x_BLE_Stack_full_fw.bin

Size : 170604 Bytes

Address : 0x08056000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [86 127]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:04.664

Firmware Upgrade process started ...

Application is running, Please Hold on...

Reconnecting...

Reconnected !

Error: The FUS version you're trying to install is older/equal to the FUS versio

n already installed !

Error: fwupgrade Command Failure!

Firwmware upgrade failed! Deleting firmware and exiting...

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

File : 0x495_FUS_Operator.bin

Size : 8 KBytes

Address : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

failed to erase memory

failed to erase memory

Failed to download FUS operator!

Could not start firmware upgrade service, old firmware delete failed

Any suggestions to fix this issue ?

This topic has been closed for replies.

20 replies

Mike_ST
ST Technical Moderator
June 16, 2021

Hello,

>> Error: Could not execute fwupgrade command, Impossible to install FUS V1.0.1 on

>> 256/512KB Flash Parts

What STM32WB firmware package do you use ?

In STM32WB firmware package V1.11.1, FUS version should be v1.2.0 not V1.0.1

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
DAlek
DAlekAuthor
Associate II
June 16, 2021

>> What STM32WB firmware package do you use ?

STM32CubeWB v1.11.1 

With stm32wb5x_FUS_fw.bin from STM32CubeWB v1.11.0, was able to update the FUS to V1.1.2.0, still unable to upload the wireless stack:

>STM32_Programmer_CLI.exe -c port=swd mode=UR -fwupgrade stm32wb5x_BLE_Stack_full_fw.bin 0x08056000 firstinstall=0

Error: The FUS version you're trying to install is older/equal to the FUS version already installed !

Error: fwupgrade Command Failure!

Firwmware upgrade failed! Deleting firmware and exiting...

Mike_ST
ST Technical Moderator
June 16, 2021

I don't know more.

Maybe @Remi QUINTIN​ can help ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Remi QUINTIN
ST Technical Moderator
June 16, 2021

There was an issue with CubeProgrammer 2.7 with 256K WB variant.

Could you revert to CubeProgrammer v2.6 and try again?

I dont think it is a FUS issue.

Could you tell me the FUS version on your board? It looks like being v1.1.1 but you can read it using CubeProgrammer en USB DFU mode.

Mike_ST
ST Technical Moderator
June 16, 2021

@Remi QUINTIN​

V1.1.2.0

he wrote that earlier:

>> With stm32wb5x_FUS_fw.bin from STM32CubeWB v1.11.0, was able to update the FUS to V1.1.2.0, still unable to upload the wireless stack:

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Remi QUINTIN
ST Technical Moderator
June 16, 2021

Strange as the FUS version available in the V1.11 package is the FUS v1.2.0.

Mike_ST
ST Technical Moderator
June 16, 2021

I don't think so, from WB packages release notes:

V1.11.0 contains FUS 1.1.2 - 02/05/2021

V1.11.1 contains FUS 1.2.0 - 04/06/2021

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Remi QUINTIN
ST Technical Moderator
June 16, 2021

Indeed you are right. I am using v1.11.1

Back to the original issue, I know there is an issue with CubeProgrammer v2.7 with 256KB WB variant.

It should be solved in the next release V2.8 expected in a few weeks (less than a month).

DAlek
DAlekAuthor
Associate II
June 17, 2021

I tried to erase completely the chip as well as change Option Bytes – User Configuration and the flash is not anymore programmable. Currently, address 0x58004020 has value of 0x000001AA. , When try to change any bit, for example, nBOOT0, errors appear:

...

08:20:22 : OPTION BYTE PROGRAMMING VERIFICATION:

08:20:22 : Error: Expected value for Option Byte "nBOOT0": 0x1, found: 0x0

08:20:23 : Error: Option Byte Programming failed

Read FUS info:

08:22:57 : Read FUS state Operation Failure! Please, try again

Firmware Upgrade:

08:26:17 : Failed to set nSWboot0=0 nboot1=1 nboot0=1

Erase & Programming:

08:31:24 : Memory Programming ...

08:31:24 : Opening and parsing file: firmware.hex

08:31:24 : File : firmware.hex

08:31:24 : Size : 395092 Bytes

08:31:24 : Address : 0x08000000

08:31:24 : Erasing memory corresponding to segment 0:

08:31:24 : Erasing internal memory sectors [0 96]

08:31:24 : Error: failed to erase memory

08:31:24 : Error: failed to erase memory

Any way to recover the flash programming and restore the initial settings ?

Remi QUINTIN
ST Technical Moderator
June 17, 2021

Just to confirm, all commands listed above were sent via CubeProgrammer v1.6 => Correct?

Your board is the Nucleo board => correct?

Could you download all the option bytes to get an exact view of the state of the board? I am afraid your board is blocked.

Revisit the logs, your device is a 512KB WB variant. So, using CubeProgrammer v1.7 should not be an issue.

All download address should be adapted accordingly vs the WB FW version. The address for the BLE full stack is not the same for WB FW v1.10 and V1.11. But I don’t see this as a cause for all those failures.

This error message is weird “Error: The FUS version you're trying to install is older/equal to the FUS version already installed !�? as you are trying to install the FW not the FUS!!!

Another one “FUS Status: FUS_FW_ROLLBACK_ERROR�? looks like the command is understood as a FUS update … strange!!!

I see you try to modify some option bytes via a direct access to the related registers. This should be ok though I always use the CubeProgrammer tool to modify them.

To read the FUS state, you have to send the command twice to ensure the FUS is really active and has updated its information.

In last resort you can try to write the value 0X00008000 at address 0x58000040C (if you can do it) and then reset the board. This action set the board back to its manufactory state (except for the FUS which remains unchanged vs the last update).

Mike_ST
ST Technical Moderator
June 17, 2021

"Just to confirm, all commands listed above were sent via CubeProgrammer v1.6 => Correct?"

Just for accuracy, v2.6 is requested not v1.6.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Remi QUINTIN
ST Technical Moderator
June 17, 2021

Correct. I wanted to write v2.6.

Remi QUINTIN
ST Technical Moderator
June 17, 2021

Never try to upgrade the FUS with a previous version.

Considering your FUS version v1.1.2, the only upgrade you could do is FUS v1.2 available the WB FW V1.11.1 package

The FUS is not device dependant except for its loading address.

What are the value of SFSA and SBRV option bytes?

DAlek
DAlekAuthor
Associate II
June 17, 2021

> Considering your FUS version v1.1.2, the only upgrade you could do is FUS v1.2 available the WB FW V1.11.1 package

Unable to upgrade the FUS from WB FW V1.11.1 package:

 13:11:07 : Error: Could not execute firmware upgrade command, Impossible to install FUS V1.0.1 on 256/512KB Flash Parts

> What are the value of SFSA and SBRV option bytes?

  Security Configuration Option bytes - 2:

   SFSA    : 0xF4 (0x80F4000)

   FSD     : 0x0 (System and Flash secure)

   DDS     : 0x1 (CPU2 debug access disabled)

   C2OPT    : 0x1 (SBRV will address Flash)

   NBRSD    : 0x0 (SRAM2b is secure)

   SNBRSA   : 0x10 (0x2003C000)

   BRSD    : 0x1 (SRAM2a is non-secure)

   SBRSA    : 0x0 (0x20030000)

   SBRV    : 0x3D000 (0x20000000)

Remi QUINTIN
ST Technical Moderator
June 17, 2021

The 2 options bytes are OK.

The error message is completely dumb "Error: Could not execute firmware upgrade command, Impossible to install FUS V1.0.1 on 256/512KB Flash Parts"

This would mean the FUS is not able to recognize the version of a new FUS!!!

I am running out of ideas ...

I will log an internal ticket for the tool team and security team to clarify this issue.

DAlek
DAlekAuthor
Associate II
June 29, 2021

Any update from the tool and security teams ?