cancel
Showing results for 
Search instead for 
Did you mean: 

TIM DMA Burst works in incorrect sequence,

xzi.1
Associate

I use tim dma burst to update CCRx(x=1\2\3\4),my code works,but the CCRx value not assigned in correct sequence. My purpose is to let CCR1= 360�?CCR2= 720�?CCR3=1080.

But the result are random.0693W00000AMamoQAD.pngTIM and DMA config codes

void tim_config()

{

uint32_t address = 0;

uint16_t i =0;

for(i=0;i<80;i++)

{

uint16_t v = 0;

v = (i%4)*10;

dmaCCBuf[i] = 36*(v+10);

}

LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);

address = TIM1_DMAR_ADDRESS;

LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_5, (uint32_t)dmaCCBuf, address, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);

LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_5, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);

LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_5, 4);

LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MEMORY_INCREMENT);

LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PERIPH_NOINCREMENT);

LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MODE_NORMAL);//

LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PRIORITY_VERYHIGH);

LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PDATAALIGN_HALFWORD);

LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MDATAALIGN_HALFWORD);

LL_TIM_ConfigDMABurst(TIM1, LL_TIM_DMABURST_BASEADDR_CCR1, LL_TIM_DMABURST_LENGTH_4TRANSFERS);

LL_TIM_EnableDMAReq_UPDATE(TIM1);

LL_TIM_EnableIT_UPDATE(TIM1);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH1);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH1N);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH2);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH2N);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH3);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH3N);

LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH4);

LL_TIM_SetTriggerOutput(TIM1, LL_TIM_TRGO_OC4REF);

//LL_TIM_SetTriggerOutput(TIM1, LL_TIM_TRGO_UPDATE);

LL_TIM_EnableARRPreload(TIM1);

LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH1);

LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH2);

LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH3);

LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH4);

LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_5);

LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_5);

NVIC_SetPriority(DMA1_Channel5_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));

NVIC_EnableIRQ(DMA1_Channel5_IRQn);

LL_TIM_EnableCounter(TIM1);

}

​DMA Interupt to restart once transfer

/* USER CODE BEGIN 1 */

void DMA1_Channel5_IRQHandler(void)

{

LL_GPIO_SetOutputPin(GPIOC, LL_GPIO_PIN_12);

LL_GPIO_ResetOutputPin(GPIOC, LL_GPIO_PIN_12);

if(LL_DMA_IsActiveFlag_TC5(DMA1))

{  

LL_DMA_ClearFlag_TC5(DMA1);

LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_5);

LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_5, 4);

LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_5);

sFlag = 1;

}

}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Don't observe TIMx_DMAR in debugger. Debugger is intrusive and reading DMAR in it advanced the internal counter/pointer to the individual TIM registers.

JW

View solution in original post

2 REPLIES 2

Don't observe TIMx_DMAR in debugger. Debugger is intrusive and reading DMAR in it advanced the internal counter/pointer to the individual TIM registers.

JW

xzi.1
Associate

Oh,Thanks very much. you are right! This program run ok!