cancel
Showing results for 
Search instead for 
Did you mean: 

Hello Dear ST Community I am Salih, Electrical Electronics Engineer and Software Developer. I am developing software for functional security in the automotive industry in a company.

MKara.7
Associate

For this reason, we need an Eval Board that meets the requirements I will list below. I request your suggestion equipment.

Thank you,

Requirements;

There must be a debugger for the uC on the development board.

uC must have Ethernet, FlexRay, USB, SDHC, CAN, LIN, UART / SCI, and SPI communication networks.

uC ISO 26262 must support at least ASIL B in terms of functional safety.

32bit uCs should be preferred for system efficiency.

uC should operate at a speed of at least 80 MHz.

1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Hello,

USB interface is not available for ST Automotive Microcontrollers. If USB interface is mandatory, then you have to look at ST Automotive Microprocessors (Accordo)

SDHC is only available on SPC58NH (high-end microcontroller)

Considering the other requirements, have a look at:

Regards,

Giuseppe

View solution in original post

1 REPLY 1
Giuseppe DI-GIORE
ST Employee

Hello,

USB interface is not available for ST Automotive Microcontrollers. If USB interface is mandatory, then you have to look at ST Automotive Microprocessors (Accordo)

SDHC is only available on SPC58NH (high-end microcontroller)

Considering the other requirements, have a look at:

Regards,

Giuseppe