Skip to main content
ranran
Senior
Sep 22, 2019 8:02 AM UTC
Question

FMC accessed in 32-bit, but CS asserted for twice long (64-bits)

Hello,

We access FMC PSRAM in 32-bits.

We noticed that although the access was expected to be in 32-bits (using HAL_SRAM_Read_32b) , CS signal is actually asserted for long of 64-bits!

Is there anything which can explain why the CS is twice the time of the expected access ?

This is the initialization of this interface of bank #3.

As you can see access is also using no wait signal:

{
 FMC_NORSRAM_TimingTypeDef Timing;
 g_hfpga.Instance = FMC_NORSRAM_DEVICE;
 g_hfpga.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
 /* g_hfpga.Init , page 821 in reference */
 g_hfpga.Init.NSBank = FMC_NORSRAM_BANK2;
 g_hfpga.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
 g_hfpga.Init.MemoryType = FMC_MEMORY_TYPE_PSRAM;
 g_hfpga.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16; 
 g_hfpga.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_ENABLE; //This bit enables/disables synchronous accesses during read operations
 g_hfpga.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
 g_hfpga.Init.WaitSignalActive = FMC_WAIT_TIMING_DURING_WS; 
 g_hfpga.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
 g_hfpga.Init.WaitSignal = FMC_WAIT_SIGNAL_ENABLE; 
 g_hfpga.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; 
 g_hfpga.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE; 
 g_hfpga.Init.WriteBurst = FMC_WRITE_BURST_ENABLE; //<-- this enables synchronous mode
 g_hfpga.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ASYNC; bank1.ContinuousClock
 g_hfpga.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
 g_hfpga.Init.PageSize = FMC_PAGE_SIZE_NONE;
 Timing.AddressSetupTime = 7;
 Timing.AddressHoldTime = 7; 
 Timing.DataSetupTime = 50;
 Timing.BusTurnAroundDuration = 4;
 Timing.CLKDivision = 4; //~200Mhz is clock source
 Timing.DataLatency = 4; 
 Timing.AccessMode = FMC_ACCESS_MODE_A; 
...
 
}

Read access timing diagram:

0690X00000ARTnrQAH.jpg

Thank you,

ran

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Sep 22, 2019 11:44 AM UTC

The bus is 16 bits wide and you're doing a 32 bit access?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ranran
ranranAuthor
Senior
Sep 22, 2019 4:19 PM UTC

mhhh , yes.

So, that's seems like a big error....

waclawek.jan
Super User
Sep 22, 2019 12:07 PM UTC
ranran
ranranAuthor
Senior
Sep 22, 2019 4:18 PM UTC

Right, sorry.

Yes, it is stm32h743.

What is the link ? Is it answering this issue ?

Thanks

Tesla DeLorean
Guru
Sep 22, 2019 4:32 PM UTC

You present information through a key-hole making the complete context hard to understand or replicate properly.

The cited thread indicates you need to watch the MPU configuration so behaviour of the caching, write-buffering, etc the core is using don't cloud the interaction on the external bus.

The poster(s) there are trying to use simplistic memory-mapped hardware, where write-thru occurs immediately and in-order.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ranran
ranranAuthor
Senior
Sep 24, 2019 6:57 AM UTC

Hi Clive,

You previously said that the bus is 16 bits wide

MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;

, and the access is 32 bit access

HAL_SRAM_Read_32b

Do you mean that it is illegal ?

Thank you!