cancel
Showing results for 
Search instead for 
Did you mean: 

Using same hex files on STM32F373 - C8T6 and STM32F373 - CCT6

NT.3
Associate II

Hi,

I developped an application using a STM32F373C8T6, but now it's time to go to production I found a very affordable source for the STM32F373CCT6.

As far as I know, it's the same chip, the CC version only has more memory.

Can I use the same hex file on both ? I don't need to access more memory than the C8 has.

I made the firmware using CubeMX.

Thanks in advance!

1 REPLY 1

The final responsibility is yours, but yes, it's the same chip, same footprint, differing only in memory - should work.

JW