cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157C-DK2 Modify, rebuild and reload a firmware CM4 example

ECaba
Associate II

Hello, I trying to make the example in: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware

but after SSH password window (here i put root in password) I get another window (attached), I don't know what pass i need to put, root don't work. (192.168.1.6 is my board ip).

Thanks.

3 REPLIES 3
PatrickF
ST Employee

Did you enter 'root' at both User and Password on the first SSH windows ? Sound strange to have edgar@192.168.1.6, should be root@192.168.1.6

Maybe have a look also to https://wiki.st.com/stm32mpu/wiki/How_to_perform_ssh_connection

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ECaba
Associate II

Hello, I used your link and I get:

0690X000009ZfjeQAC.png

Next I in workbench my debug configuration is:0690X000009ZfjkQAC.png

I next dialog: user and pass are: root

0690X000009ZfjyQAC.png

For last I get one more dialog:

0690X000009Zfk8QAC.png

What should i put here?, if I click in CANCEL the debug session fail.

Thanks

Secure storage is an Eclipse feature (System Workbench for STM32 is based on Eclipse)

To deactivate Secure storage, please do following steps :

  1. Windows->preferences->then type "secure storage"
  2. In the Contents tab, select [Default Secure Storage].
  3. Click Delete.
  4. Let Eclipse restart.

About login/password, you should use "root" as login but with no password