cancel
Showing results for 
Search instead for 
Did you mean: 

Core toggles between “Core running�? and “Core inactive�? this indicates continuous reset.

sraga.1
Associate

We are using SPC560D40L3 micro-control.

When powered on we see a continuous reset of the board.

Core toggles between “Core running�? and “Core inactive�? this indicates continuous reset.

Following is the snapshot of debugger window.

Controller does not even allow to re flash or set break point.

This being an urgent issue I urge your prompt support.

warning message

, Warning, Core::PpcJtagTargIntf, This was caused probably by application (destructive reset) or external tool.

0 REPLIES 0